EmbossTaper Class¶
-
class
NXOpen.Features.
EmbossTaper
¶ Bases:
NXOpen.TaggedObject
Represents a taper object.
This class provides methods to set and get taper angle.
Following is default values:
**Taper Angle</b> 5.0 degrees
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns the emboss taper angle |
BackAngle | Returns the emboss back taper angle the back angle expression |
Tag | Returns the Tag for this object. |
Property Detail¶
Angle¶
-
EmbossTaper.
Angle
¶ Returns the emboss taper angle
-------------------------------------
Getter Method
Signature
Angle
Returns: Taper angle Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: None.
BackAngle¶
-
EmbossTaper.
BackAngle
¶ Returns the emboss back taper angle the back angle expression
-------------------------------------
Getter Method
Signature
BackAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.