MultiDraftAngleOption Enumeration

NXOpen.GeometricUtilities.MultiDraft.AngleOption is an alias for NXOpen.GeometricUtilities.MultiDraftAngleOption

class NXOpen.GeometricUtilities.MultiDraftAngleOption

Bases: object

Represents the angle option.

Enum Members

Enum Member Enum Member Description
Single Sigle draft
Multiple Multi draft
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.