SurfaceContinuityAnalysisBuilder Class¶
-
class
NXOpen.GeometricAnalysis.
SurfaceContinuityAnalysisBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.GeometricAnalysis.SurfaceContinuityAnalysis
builderTo create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisObjectCollection.CreateSurfaceContinuityAnalysisBuilder()
Default values.
Property Value CurvatureCheck Sectional G0 True G1 False G2 False G3 False New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AngularThreshold | Returns the angular threshold |
CombOptions | Returns the comb display block options |
CurvatureCheck | Returns or sets the curvature check |
DistanceThreshold | Returns the distance threshold |
DynamicLabel | Returns the constraint manager |
Face | Returns the (second) faces. |
FirstEdge | Returns the first edges or faces |
G0 | Returns or sets the g0 toggle |
G0Tolerance | Returns or sets the g0 tolerance |
G1 | Returns or sets the g1 toggle |
G1Tolerance | Returns or sets the g1 tolerance |
G2 | Returns or sets the g2 toggle |
G2Tolerance | Returns or sets the g2 tolerance |
G3 | Returns or sets the g3 toggle |
G3Tolerance | Returns or sets the g3 tolerance |
MultiFace | Returns the objects for multi-face |
ReportPer | Returns or sets the reporting type |
SecondEdge | Returns the second edges or faces. |
ShowOutOfTolerance | Returns or sets the out of tolerance only flag |
Tag | Returns the Tag for this object. |
ToleranceMarkup | Returns or sets the tolerance markup flag |
Type | Returns or sets the type of analysis to perform |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DeselectFirstEdgeFace | Deselection of first edge or face |
DeselectSecondEdgeFace | Deselection of second edge or face |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFace1Array | Returns the edge1 array not used |
GetObject | Returns the object currently being edited by this builder. |
SelectFirstEdgeFace | Selection of first edge or face |
SelectSecondEdgeFace | Selection of second edge or face |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateFace | User selects or deselects face, update builder m_edge2, m_face2 |
UpdateFirstEdgeFace | The user selects or deselects first edge or face, update builder m_edge1, m_face1 |
UpdateSecondEdgeFace | User selects or deselects second edge or face, update builder m_edge2, m_face2 |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SurfaceContinuityAnalysisBuilderCurvatureType Enumeration | Curvature types |
SurfaceContinuityAnalysisBuilderReportingType Enumeration | Reporting types |
SurfaceContinuityAnalysisBuilderTypes Enumeration | Two possible types for the dialog |
Property Detail¶
AngularThreshold¶
-
SurfaceContinuityAnalysisBuilder.
AngularThreshold
¶ Returns the angular threshold
-------------------------------------
Getter Method
Signature
AngularThreshold
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
CombOptions¶
-
SurfaceContinuityAnalysisBuilder.
CombOptions
¶ Returns the comb display block options
-------------------------------------
Getter Method
Signature
CombOptions
Returns: Return type: NXOpen.GeometricUtilities.CombOptionsBuilder
New in version NX6.0.0.
License requirements: None.
CurvatureCheck¶
-
SurfaceContinuityAnalysisBuilder.
CurvatureCheck
¶ Returns or sets the curvature check
-------------------------------------
Getter Method
Signature
CurvatureCheck
Returns: Return type: NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderCurvatureType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurvatureCheck
Parameters: curvatureCheck ( NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderCurvatureType
) –New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
DistanceThreshold¶
-
SurfaceContinuityAnalysisBuilder.
DistanceThreshold
¶ Returns the distance threshold
-------------------------------------
Getter Method
Signature
DistanceThreshold
Returns: Return type: NXOpen.Expression
New in version NX11.0.0.
License requirements: None.
DynamicLabel¶
-
SurfaceContinuityAnalysisBuilder.
DynamicLabel
¶ Returns the constraint manager
-------------------------------------
Getter Method
Signature
DynamicLabel
Returns: Return type: NXOpen.Features.GeometricConstraintDataManager
New in version NX11.0.0.
License requirements: None.
Face¶
-
SurfaceContinuityAnalysisBuilder.
Face
¶ Returns the (second) faces.
Used only if the type is EdgeFace
-------------------------------------
Getter Method
Signature
Face
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
FirstEdge¶
-
SurfaceContinuityAnalysisBuilder.
FirstEdge
¶ Returns the first edges or faces
-------------------------------------
Getter Method
Signature
FirstEdge
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
G0¶
-
SurfaceContinuityAnalysisBuilder.
G0
¶ Returns or sets the g0 toggle
-------------------------------------
Getter Method
Signature
G0
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G0
Parameters: g0 (bool) – New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
G0Tolerance¶
-
SurfaceContinuityAnalysisBuilder.
G0Tolerance
¶ Returns or sets the g0 tolerance
-------------------------------------
Getter Method
Signature
G0Tolerance
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G0Tolerance
Parameters: g0Tolerance (float) – New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
G1¶
-
SurfaceContinuityAnalysisBuilder.
G1
¶ Returns or sets the g1 toggle
-------------------------------------
Getter Method
Signature
G1
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G1
Parameters: g1 (bool) – New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
G1Tolerance¶
-
SurfaceContinuityAnalysisBuilder.
G1Tolerance
¶ Returns or sets the g1 tolerance
-------------------------------------
Getter Method
Signature
G1Tolerance
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G1Tolerance
Parameters: g1Tolerance (float) – New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
G2¶
-
SurfaceContinuityAnalysisBuilder.
G2
¶ Returns or sets the g2 toggle
-------------------------------------
Getter Method
Signature
G2
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G2
Parameters: g2 (bool) – New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
G2Tolerance¶
-
SurfaceContinuityAnalysisBuilder.
G2Tolerance
¶ Returns or sets the g2 tolerance
-------------------------------------
Getter Method
Signature
G2Tolerance
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G2Tolerance
Parameters: g2Tolerance (float) – New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
G3¶
-
SurfaceContinuityAnalysisBuilder.
G3
¶ Returns or sets the g3 toggle
-------------------------------------
Getter Method
Signature
G3
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G3
Parameters: g3 (bool) – New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
G3Tolerance¶
-
SurfaceContinuityAnalysisBuilder.
G3Tolerance
¶ Returns or sets the g3 tolerance
-------------------------------------
Getter Method
Signature
G3Tolerance
Returns: Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
G3Tolerance
Parameters: g3Tolerance (float) – New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
MultiFace¶
-
SurfaceContinuityAnalysisBuilder.
MultiFace
¶ Returns the objects for multi-face
-------------------------------------
Getter Method
Signature
MultiFace
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
ReportPer¶
-
SurfaceContinuityAnalysisBuilder.
ReportPer
¶ Returns or sets the reporting type
-------------------------------------
Getter Method
Signature
ReportPer
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReportPer
Parameters: reportPer (int) – New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
SecondEdge¶
-
SurfaceContinuityAnalysisBuilder.
SecondEdge
¶ Returns the second edges or faces.
Used only if the type is EdgeEdge
-------------------------------------
Getter Method
Signature
SecondEdge
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
ShowOutOfTolerance¶
-
SurfaceContinuityAnalysisBuilder.
ShowOutOfTolerance
¶ Returns or sets the out of tolerance only flag
-------------------------------------
Getter Method
Signature
ShowOutOfTolerance
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowOutOfTolerance
Parameters: outTolerance (bool) – New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
ToleranceMarkup¶
-
SurfaceContinuityAnalysisBuilder.
ToleranceMarkup
¶ Returns or sets the tolerance markup flag
-------------------------------------
Getter Method
Signature
ToleranceMarkup
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToleranceMarkup
Parameters: markup (bool) – New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
Type¶
-
SurfaceContinuityAnalysisBuilder.
Type
¶ Returns or sets the type of analysis to perform
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderTypes
) –New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
Method Detail¶
DeselectFirstEdgeFace¶
-
SurfaceContinuityAnalysisBuilder.
DeselectFirstEdgeFace
¶ Deselection of first edge or face
Signature
DeselectFirstEdgeFace(edge, face)
Parameters: - edge (
NXOpen.DisplayableObject
) – - face (
NXOpen.DisplayableObject
) –
New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
- edge (
DeselectSecondEdgeFace¶
-
SurfaceContinuityAnalysisBuilder.
DeselectSecondEdgeFace
¶ Deselection of second edge or face
Signature
DeselectSecondEdgeFace(edge, face)
Parameters: - edge (
NXOpen.DisplayableObject
) – - face (
NXOpen.DisplayableObject
) –
New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
- edge (
GetFace1Array¶
-
SurfaceContinuityAnalysisBuilder.
GetFace1Array
¶ Returns the edge1 array not used
Signature
GetFace1Array()
Returns: Return type: list of NXOpen.Face
New in version NX6.0.0.
License requirements: None.
SelectFirstEdgeFace¶
-
SurfaceContinuityAnalysisBuilder.
SelectFirstEdgeFace
¶ Selection of first edge or face
Signature
SelectFirstEdgeFace(edge, face)
Parameters: - edge (
NXOpen.DisplayableObject
) – - face (
NXOpen.DisplayableObject
) –
New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
- edge (
SelectSecondEdgeFace¶
-
SurfaceContinuityAnalysisBuilder.
SelectSecondEdgeFace
¶ Selection of second edge or face
Signature
SelectSecondEdgeFace(edge, face)
Parameters: - edge (
NXOpen.DisplayableObject
) – - face (
NXOpen.DisplayableObject
) –
New in version NX11.0.0.
License requirements: gateway (“UG GATEWAY”)
- edge (
UpdateFace¶
-
SurfaceContinuityAnalysisBuilder.
UpdateFace
¶ User selects or deselects face, update builder m_edge2, m_face2
Signature
UpdateFace(face, selectionPoint)
Parameters: - face (
NXOpen.Face
) – - selectionPoint (
NXOpen.Point3d
) –
New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
- face (
UpdateFirstEdgeFace¶
-
SurfaceContinuityAnalysisBuilder.
UpdateFirstEdgeFace
¶ The user selects or deselects first edge or face, update builder m_edge1, m_face1
Signature
UpdateFirstEdgeFace(edgeOrFace, selectionPoint)
Parameters: - edgeOrFace (
NXOpen.DisplayableObject
) – the parent of Face or Edge - selectionPoint (
NXOpen.Point3d
) –
New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
- edgeOrFace (
UpdateSecondEdgeFace¶
-
SurfaceContinuityAnalysisBuilder.
UpdateSecondEdgeFace
¶ User selects or deselects second edge or face, update builder m_edge2, m_face2
Signature
UpdateSecondEdgeFace(edgeOrFace, selectionPoint)
Parameters: - edgeOrFace (
NXOpen.DisplayableObject
) – the parent of Face or Edge - selectionPoint (
NXOpen.Point3d
) –
New in version NX6.0.0.
License requirements: gateway (“UG GATEWAY”)
- edgeOrFace (
Validate¶
-
SurfaceContinuityAnalysisBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.