SurfaceContinuityAnalysisBuilderCurvatureType Enumeration

NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilder.CurvatureType is an alias for NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderCurvatureType

class NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderCurvatureType

Bases: object

Curvature types

Enum Members

Enum Member Enum Member Description
Sectional
Gaussian
Mean
Absolute
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.