SurfaceContinuityAnalysisBuilderReportingType Enumeration

NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilder.ReportingType is an alias for NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderReportingType

class NXOpen.GeometricAnalysis.SurfaceContinuityAnalysisBuilderReportingType

Bases: object

Reporting types

Enum Members

Enum Member Enum Member Description
Analysis
Pair
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.