GeometricProperties Class¶
-
class
NXOpen.GeometricAnalysis.
GeometricProperties
¶ Bases:
NXOpen.Builder
Represents the Geometric Properties class.
This class can be used to find local geometric properties of faces, edges, curves, CAE faces, and CAE edges/curves at a given point.
To create a new instance of this class, use
NXOpen.GeometricAnalysis.AnalysisManager.CreateGeometricPropertiesObject()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ObjectsForAnalysis | Returns the Objects for analysis |
OutputMethod | Returns or sets the output method |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCaeCurveProperties | Returns CAE curve local properties at the given point |
GetCaeFaceProperties | Returns CAE face local properties at the given point |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEdgeProperties | Returns edge/curve local properties at the given point |
GetFaceProperties | Returns face local properties at the given point |
GetObject | Returns the object currently being edited by this builder. |
ListProperties | Displays the local properties of the specified object at the given point in the listing window |
Reset | Clears all markers showing the local geometric properties in the graphics window |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
GeometricPropertiesEntity Enumeration | Type of input entity for geometric properties. |
GeometricPropertiesOutputType Enumeration | Represents how to output geometric properties. |
GeometricPropertiesStatus Enumeration | Status of computing geometric properties. |
Structs¶
GeometricPropertiesCaeCurve_Struct Struct | CAE Edge/Curve Geometric Properties |
GeometricPropertiesCaeFace_Struct Struct | CAE Face Geometric Properties |
GeometricPropertiesEdge_Struct Struct | Edge/Curve Geometric Properties |
GeometricPropertiesFace_Struct Struct | Face Geometric Properties |
Property Detail¶
ObjectsForAnalysis¶
-
GeometricProperties.
ObjectsForAnalysis
¶ Returns the Objects for analysis
-------------------------------------
Getter Method
Signature
ObjectsForAnalysis
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
OutputMethod¶
-
GeometricProperties.
OutputMethod
¶ Returns or sets the output method
-------------------------------------
Getter Method
Signature
OutputMethod
Returns: Return type: NXOpen.GeometricAnalysis.GeometricPropertiesOutputType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputMethod
Parameters: outputMethod ( NXOpen.GeometricAnalysis.GeometricPropertiesOutputType
) –New in version NX5.0.0.
License requirements: None.
Method Detail¶
GetCaeCurveProperties¶
-
GeometricProperties.
GetCaeCurveProperties
¶ Returns CAE curve local properties at the given point
Signature
GetCaeCurveProperties(entityTag, absPoint)
Parameters: - entityTag (
NXOpen.NXObject
) – NXObject to obtain the properties for - absPoint (
NXOpen.Point3d
) – Absolute point co-ordinates of the reference point to compute the properties
Returns: a tuple
Return type: A tuple consisting of (status, caeCurve). status is a
NXOpen.GeometricAnalysis.GeometricPropertiesStatus
. Return status caeCurve is aNXOpen.GeometricAnalysis.GeometricPropertiesCaeCurve_Struct
. CAE Edge/Curve PropertiesNew in version NX5.0.0.
License requirements: None.
- entityTag (
GetCaeFaceProperties¶
-
GeometricProperties.
GetCaeFaceProperties
¶ Returns CAE face local properties at the given point
Signature
GetCaeFaceProperties(entityTag, absPoint)
Parameters: - entityTag (
NXOpen.NXObject
) – NXObject to obtain the properties for - absPoint (
NXOpen.Point3d
) – Absolute point co-ordinates of the reference point to compute the properties
Returns: a tuple
Return type: A tuple consisting of (status, caeFace). status is a
NXOpen.GeometricAnalysis.GeometricPropertiesStatus
. Return status caeFace is aNXOpen.GeometricAnalysis.GeometricPropertiesCaeFace_Struct
. CAE Face PropertiesNew in version NX5.0.0.
License requirements: None.
- entityTag (
GetEdgeProperties¶
-
GeometricProperties.
GetEdgeProperties
¶ Returns edge/curve local properties at the given point
Signature
GetEdgeProperties(entityTag, absPoint)
Parameters: - entityTag (
NXOpen.NXObject
) – NXObject to obtain the properties for - absPoint (
NXOpen.Point3d
) – Absolute point co-ordinates of the reference point to compute the properties
Returns: a tuple
Return type: A tuple consisting of (status, edge). status is a
NXOpen.GeometricAnalysis.GeometricPropertiesStatus
. Return status edge is aNXOpen.GeometricAnalysis.GeometricPropertiesEdge_Struct
. Edge/Curve PropertiesNew in version NX5.0.0.
License requirements: None.
- entityTag (
GetFaceProperties¶
-
GeometricProperties.
GetFaceProperties
¶ Returns face local properties at the given point
Signature
GetFaceProperties(entityTag, absPoint)
Parameters: - entityTag (
NXOpen.NXObject
) – NXObject to obtain the properties for - absPoint (
NXOpen.Point3d
) – Absolute point co-ordinates of the reference point to compute the properties
Returns: a tuple
Return type: A tuple consisting of (status, face). status is a
NXOpen.GeometricAnalysis.GeometricPropertiesStatus
. Return status face is aNXOpen.GeometricAnalysis.GeometricPropertiesFace_Struct
. Face PropertiesNew in version NX5.0.0.
License requirements: None.
- entityTag (
ListProperties¶
-
GeometricProperties.
ListProperties
¶ Overloaded method ListProperties
ListProperties(entityTag, absPoint)
ListProperties(absPoint)
-------------------------------------
Displays the local properties of the specified object at the given point in the listing window
Signature
ListProperties(entityTag, absPoint)
Parameters: - entityTag (
NXOpen.NXObject
) – NXObject to obtain the properties for - absPoint (
NXOpen.Point3d
) – Absolute point co-ordinates of the reference point to compute the properties
Returns: Return status
Return type: New in version NX5.0.0.
License requirements: None.
-------------------------------------
Displays the local properties of
ObjectsForAnalysis()
at the given point in the listing window.Signature
ListProperties(absPoint)
Parameters: absPoint ( NXOpen.Point3d
) – Absolute point co-ordinates of the reference point to compute the propertiesReturns: Return status Return type: NXOpen.GeometricAnalysis.GeometricPropertiesStatus
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Reset¶
-
GeometricProperties.
Reset
¶ Clears all markers showing the local geometric properties in the graphics window
Signature
Reset()
New in version NX5.0.0.
License requirements: None.
Validate¶
-
GeometricProperties.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.