GeometricPropertiesOutputType Enumeration¶
NXOpen.GeometricAnalysis.GeometricProperties.OutputType is an alias for NXOpen.GeometricAnalysis.GeometricPropertiesOutputType
-
class
NXOpen.GeometricAnalysis.
GeometricPropertiesOutputType
¶ Bases:
object
Represents how to output geometric properties.
GeometricAnalysis.GeometricPropertiesOutputType.Dynamic
displays the properties of an entity under the cursor when NX is run interactively.Enum Members
Enum Member Enum Member Description Dynamic Properties of an entity are displayed first on the dialog itself on mouse over. These properties are listed on in the information window upon selection of a point. Static Propeties of the selected entities are displayed in the information window. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-