GeometricPropertiesCaeFace_Struct Struct

NXOpen.GeometricAnalysis.GeometricProperties.CaeFace is an alias for NXOpen.GeometricAnalysis.GeometricPropertiesCaeFace_Struct

class NXOpen.GeometricAnalysis.GeometricPropertiesCaeFace_Struct

Bases: object

CAE Face Geometric Properties .

Constructor: NXOpen.GeometricAnalysis.GeometricProperties.CaeFace()

Fields

Field Description
ClosestPoint closest point on face in Root Part Coordinates
UParameter u parameter of the closest point in Root Part Coordinates
VParameter v parameter of the closest point in Root Part Coordinates
Normal normal at the closest point in Root Part Coordinates
ClosestPointInWcs closest point in Work Part Coordinates
NormalInWcs normal in Work Part Coordinates
UDerivative Derivative in U, Root Part Coordinates
VDerivative Derivative in V, Root Part Coordinates
UDerivativeInWcs Derivative in U in Work Part Coordinates
VDerivativeInWcs Derivative in V in Work Part Coordinates

ClosestPoint

GeometricPropertiesCaeFace_Struct.ClosestPoint

closest point on face in Root Part Coordinates -------------------------------------

Field Value Type:NXOpen.Vector3d

UParameter

GeometricPropertiesCaeFace_Struct.UParameter

u parameter of the closest point in Root Part Coordinates -------------------------------------

Field Value Type:float

VParameter

GeometricPropertiesCaeFace_Struct.VParameter

v parameter of the closest point in Root Part Coordinates -------------------------------------

Field Value Type:float

Normal

GeometricPropertiesCaeFace_Struct.Normal

normal at the closest point in Root Part Coordinates -------------------------------------

Field Value Type:NXOpen.Vector3d

ClosestPointInWcs

GeometricPropertiesCaeFace_Struct.ClosestPointInWcs

closest point in Work Part Coordinates -------------------------------------

Field Value Type:NXOpen.Point3d

NormalInWcs

GeometricPropertiesCaeFace_Struct.NormalInWcs

normal in Work Part Coordinates -------------------------------------

Field Value Type:NXOpen.Vector3d

UDerivative

GeometricPropertiesCaeFace_Struct.UDerivative

Derivative in U, Root Part Coordinates -------------------------------------

Field Value Type:NXOpen.Vector3d

VDerivative

GeometricPropertiesCaeFace_Struct.VDerivative

Derivative in V, Root Part Coordinates -------------------------------------

Field Value Type:NXOpen.Vector3d

UDerivativeInWcs

GeometricPropertiesCaeFace_Struct.UDerivativeInWcs

Derivative in U in Work Part Coordinates -------------------------------------

Field Value Type:NXOpen.Vector3d

VDerivativeInWcs

GeometricPropertiesCaeFace_Struct.VDerivativeInWcs

Derivative in V in Work Part Coordinates -------------------------------------

Field Value Type:NXOpen.Vector3d