CloseRangeVisibilityBuilder Class¶
-
class
NXOpen.Features.VehicleDesign.
CloseRangeVisibilityBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
The builder to create close range visibility feature.
To create a new instance of this class, use
NXOpen.Features.VehicleDesignCollection.CreateCloseRangeVisibilityBuilder()
Default values.
Property Value CylinderHeight.Value 1000 (millimeters part), 40 (inches part) CylinderRadius.Value 150 (millimeters part), 6 (inches part) DistanceFromVehicle.Value 2000 (millimeters part), 78.7 (inches part) DriverSideExtension.Value 700 (millimeters part), 27.5 (inches part) EyePointOffsetType NoOffset EyePointType Binocular K1Coefficient.Value 0.292 K2Coefficient.Value 203 (millimeters part), 7.99 (inches part) MirrorRotationYAngle.Value 0 MirrorRotationZAngle.Value 0 PassengerSideExtension.Value 900 (millimeters part), 35.4 (inches part) PathPositionType Both PositionMethod TangentArea PositionPath BaseData RequirementsControl StandardDriven RotateMirrorFace 0 ShowBlindVolume 0 ShowExtendedEyes 0 ShowEyeLabels 0 ShowEyePoints 0 ShowPath 0 ShowPathPoints 0 ShowSightRays 0 ShowTorsoLine 0 StepValue 0.5 UseMirror 0 New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CameraList | Returns the list of NXOpen.Features.VehicleDesign.CloseRangeCameraListItemBuilder defining the camera parameters. |
CylinderHeight | Returns the expression containing the value for the cylinder height. |
CylinderRadius | Returns the expression containing the value for the cylinder radius. |
DemoCylinderList | Returns the list of NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilder defining the demo cylinder parameters. |
DistanceFromVehicle | Returns the expression containing the value for the distance from vehicle. |
DriverSideExtension | Returns the expression containing the value for the driver side extension. |
EyePointOffsetType | Returns or sets the eye point offset types to define the close range visibility. |
EyePointType | Returns or sets the eye point types to define the close range visibility. |
K1Coefficient | Returns the expression containing the value for the k1 coefficient used in blind volume checking. |
K2Coefficient | Returns the expression containing the value for the k2 coefficient used in blind volume checking. |
Loading | Returns or sets the loading used in the close range visibility. |
MirrorBoundary | Returns the curves selection used to identify the mirror boundary section. |
MirrorFaces | Returns the faces selection used to identify the mirror surfaces. |
MirrorFacetBodies | Returns the facet selection used to identify the mirror facet bodies. |
MirrorRotationPoint | Returns or sets the mirror rotation point specified. |
MirrorRotationYAngle | Returns the mirror rotation angle around vehicle Y axis after Z axis. |
MirrorRotationZAngle | Returns the mirror rotation angle around vehicle Z axis. |
ObstructionFaces | Returns the faces selection used to identify the vehicle obstruction surfaces. |
ObstructionFacetBodies | Returns the faces selection used to identify the vehicle obstruction facet bodies. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PassengerSideExtension | Returns the expression containing the value for the passenger side extension. |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PathPositionType | Returns or sets the path position types used to define close range visibility. |
PositionMethod | Returns or sets the position method types to define the close range visibility. |
PositionPath | Returns or sets the position path types to define the close range visibility. |
RequirementsControl | Returns or sets the requirements control types to define the close range visibility. |
RotateMirrorFace | Returns or sets the indication if the mirror face will be rotated. |
ShowBlindVolume | Returns or sets the indication if blind volume will be displayed. |
ShowExtendedEyes | Returns or sets the indication if extended eyes will be displayed. |
ShowEyeLabels | Returns or sets the indication if eye labels will be displayed. |
ShowEyePoints | Returns or sets the indication if eye points will be displayed. |
ShowPath | Returns or sets the indication if demo cylinder path will be displayed. |
ShowPathPoints | Returns or sets the indication if demo cylinder point position on path will be displayed. |
ShowSightRays | Returns or sets the indication if blind volume sight rays will be displayed. |
ShowTorsoLine | Returns or sets the indication if torso line will be displayed. |
Standard | Returns or sets the standard types to define the close range visibility. |
StepValue | Returns or sets the step value to control the accurate for demo cylinder visibility and blind volume area calculation. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
UseMirror | Returns or sets the indication if the mirror will be used. |
VehicleBodies | Returns the bodies selection used to identify vehicle bodies. |
VehicleFacetBodies | Returns the bodies selection used to identify vehicle facet bodies. |
WindowFaces | Returns the faces selection used to identify the vehicle window surfaces. |
WindowFacetBodies | Returns the faces selection used to identify the vehicle window facet bodies. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreateCameraListItemBuilder | Creates a NXOpen.Features.VehicleDesign.CloseRangeCameraListItemBuilder |
CreateDemoCylinderListItemBuilder | Creates a NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilder |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBlindVolumes | Validate blind volume area from driver side view. |
Enumerations¶
CloseRangeVisibilityBuilderEyePointOffsetTypes Enumeration | This enum represents the eye position offset options. |
CloseRangeVisibilityBuilderEyePointTypes Enumeration | This enum represents the binocular or monocular eye position definition options. |
CloseRangeVisibilityBuilderPathPositionTypes Enumeration | This enum represents the cylinder path position display options. |
CloseRangeVisibilityBuilderPositionMethods Enumeration | This enum represents the cylinder position method options. |
CloseRangeVisibilityBuilderPositionPaths Enumeration | This enum represents the cylinder position path options. |
CloseRangeVisibilityBuilderRequirementsControlType Enumeration | This enum represents the standard or user defined requirement options. |
Property Detail¶
CameraList¶
-
CloseRangeVisibilityBuilder.
CameraList
¶ Returns the list of
NXOpen.Features.VehicleDesign.CloseRangeCameraListItemBuilder
defining the camera parameters.-------------------------------------
Getter Method
Signature
CameraList
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeCameraListItemBuilderList
New in version NX8.5.0.
License requirements: None.
CylinderHeight¶
-
CloseRangeVisibilityBuilder.
CylinderHeight
¶ Returns the expression containing the value for the cylinder height.
-------------------------------------
Getter Method
Signature
CylinderHeight
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
CylinderRadius¶
-
CloseRangeVisibilityBuilder.
CylinderRadius
¶ Returns the expression containing the value for the cylinder radius.
-------------------------------------
Getter Method
Signature
CylinderRadius
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
DemoCylinderList¶
-
CloseRangeVisibilityBuilder.
DemoCylinderList
¶ Returns the list of
NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilder
defining the demo cylinder parameters.-------------------------------------
Getter Method
Signature
DemoCylinderList
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilderList
New in version NX8.5.0.
License requirements: None.
DistanceFromVehicle¶
-
CloseRangeVisibilityBuilder.
DistanceFromVehicle
¶ Returns the expression containing the value for the distance from vehicle.
Only valid when position method equals to front view type.
-------------------------------------
Getter Method
Signature
DistanceFromVehicle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
DriverSideExtension¶
-
CloseRangeVisibilityBuilder.
DriverSideExtension
¶ Returns the expression containing the value for the driver side extension.
Only valid when position method equals to front view type.
-------------------------------------
Getter Method
Signature
DriverSideExtension
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
EyePointOffsetType¶
-
CloseRangeVisibilityBuilder.
EyePointOffsetType
¶ Returns or sets the eye point offset types to define the close range visibility.
-------------------------------------
Getter Method
Signature
EyePointOffsetType
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderEyePointOffsetTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyePointOffsetType
Parameters: eyePointOffsetType ( NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderEyePointOffsetTypes
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
EyePointType¶
-
CloseRangeVisibilityBuilder.
EyePointType
¶ Returns or sets the eye point types to define the close range visibility.
-------------------------------------
Getter Method
Signature
EyePointType
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderEyePointTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EyePointType
Parameters: eyePointType ( NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderEyePointTypes
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
K1Coefficient¶
-
CloseRangeVisibilityBuilder.
K1Coefficient
¶ Returns the expression containing the value for the k1 coefficient used in blind volume checking.
-------------------------------------
Getter Method
Signature
K1Coefficient
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
K2Coefficient¶
-
CloseRangeVisibilityBuilder.
K2Coefficient
¶ Returns the expression containing the value for the k2 coefficient used in blind volume checking.
-------------------------------------
Getter Method
Signature
K2Coefficient
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
Loading¶
-
CloseRangeVisibilityBuilder.
Loading
¶ Returns or sets the loading used in the close range visibility.
-------------------------------------
Getter Method
Signature
Loading
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Loading
Parameters: loading (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
MirrorBoundary¶
-
CloseRangeVisibilityBuilder.
MirrorBoundary
¶ Returns the curves selection used to identify the mirror boundary section.
Only valid when use mirror is checked.
-------------------------------------
Getter Method
Signature
MirrorBoundary
Returns: Return type: NXOpen.Section
New in version NX8.5.0.
License requirements: None.
MirrorFaces¶
-
CloseRangeVisibilityBuilder.
MirrorFaces
¶ Returns the faces selection used to identify the mirror surfaces.
Only valid when use mirror is checked.
-------------------------------------
Getter Method
Signature
MirrorFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
MirrorFacetBodies¶
-
CloseRangeVisibilityBuilder.
MirrorFacetBodies
¶ Returns the facet selection used to identify the mirror facet bodies.
Only valid when use mirror is checked.
-------------------------------------
Getter Method
Signature
MirrorFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
MirrorRotationPoint¶
-
CloseRangeVisibilityBuilder.
MirrorRotationPoint
¶ Returns or sets the mirror rotation point specified.
Only valid when rotate mirror face is checked.
-------------------------------------
Getter Method
Signature
MirrorRotationPoint
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MirrorRotationPoint
Parameters: mirrorRotationPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
MirrorRotationYAngle¶
-
CloseRangeVisibilityBuilder.
MirrorRotationYAngle
¶ Returns the mirror rotation angle around vehicle Y axis after Z axis.
Only valid when rotate mirror face is checked.
-------------------------------------
Getter Method
Signature
MirrorRotationYAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
MirrorRotationZAngle¶
-
CloseRangeVisibilityBuilder.
MirrorRotationZAngle
¶ Returns the mirror rotation angle around vehicle Z axis.
Only valid when rotate mirror face is checked.
-------------------------------------
Getter Method
Signature
MirrorRotationZAngle
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
ObstructionFaces¶
-
CloseRangeVisibilityBuilder.
ObstructionFaces
¶ Returns the faces selection used to identify the vehicle obstruction surfaces.
-------------------------------------
Getter Method
Signature
ObstructionFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
ObstructionFacetBodies¶
-
CloseRangeVisibilityBuilder.
ObstructionFacetBodies
¶ Returns the faces selection used to identify the vehicle obstruction facet bodies.
-------------------------------------
Getter Method
Signature
ObstructionFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
PassengerSideExtension¶
-
CloseRangeVisibilityBuilder.
PassengerSideExtension
¶ Returns the expression containing the value for the passenger side extension.
Only valid when position method equals to front view type.
-------------------------------------
Getter Method
Signature
PassengerSideExtension
Returns: Return type: NXOpen.Expression
New in version NX8.5.0.
License requirements: None.
PathPositionType¶
-
CloseRangeVisibilityBuilder.
PathPositionType
¶ Returns or sets the path position types used to define close range visibility.
-------------------------------------
Getter Method
Signature
PathPositionType
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderPathPositionTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PathPositionType
Parameters: pathPositionType ( NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderPathPositionTypes
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PositionMethod¶
-
CloseRangeVisibilityBuilder.
PositionMethod
¶ Returns or sets the position method types to define the close range visibility.
-------------------------------------
Getter Method
Signature
PositionMethod
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderPositionMethods
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositionMethod
Parameters: positionMethod ( NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderPositionMethods
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
PositionPath¶
-
CloseRangeVisibilityBuilder.
PositionPath
¶ Returns or sets the position path types to define the close range visibility.
-------------------------------------
Getter Method
Signature
PositionPath
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderPositionPaths
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositionPath
Parameters: positionPath ( NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderPositionPaths
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RequirementsControl¶
-
CloseRangeVisibilityBuilder.
RequirementsControl
¶ Returns or sets the requirements control types to define the close range visibility.
-------------------------------------
Getter Method
Signature
RequirementsControl
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderRequirementsControlType
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RequirementsControl
Parameters: requirement ( NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderRequirementsControlType
) –New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
RotateMirrorFace¶
-
CloseRangeVisibilityBuilder.
RotateMirrorFace
¶ Returns or sets the indication if the mirror face will be rotated.
Only valid when use mirror is checked.
-------------------------------------
Getter Method
Signature
RotateMirrorFace
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RotateMirrorFace
Parameters: rotateMirrorFace (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowBlindVolume¶
-
CloseRangeVisibilityBuilder.
ShowBlindVolume
¶ Returns or sets the indication if blind volume will be displayed.
-------------------------------------
Getter Method
Signature
ShowBlindVolume
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowBlindVolume
Parameters: showBlindVolume (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowExtendedEyes¶
-
CloseRangeVisibilityBuilder.
ShowExtendedEyes
¶ Returns or sets the indication if extended eyes will be displayed.
-------------------------------------
Getter Method
Signature
ShowExtendedEyes
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowExtendedEyes
Parameters: showExtendedEyes (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowEyeLabels¶
-
CloseRangeVisibilityBuilder.
ShowEyeLabels
¶ Returns or sets the indication if eye labels will be displayed.
-------------------------------------
Getter Method
Signature
ShowEyeLabels
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowEyeLabels
Parameters: showEyeLabels (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowEyePoints¶
-
CloseRangeVisibilityBuilder.
ShowEyePoints
¶ Returns or sets the indication if eye points will be displayed.
-------------------------------------
Getter Method
Signature
ShowEyePoints
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowEyePoints
Parameters: showEyePoints (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowPath¶
-
CloseRangeVisibilityBuilder.
ShowPath
¶ Returns or sets the indication if demo cylinder path will be displayed.
-------------------------------------
Getter Method
Signature
ShowPath
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowPath
Parameters: showPath (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowPathPoints¶
-
CloseRangeVisibilityBuilder.
ShowPathPoints
¶ Returns or sets the indication if demo cylinder point position on path will be displayed.
-------------------------------------
Getter Method
Signature
ShowPathPoints
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowPathPoints
Parameters: showPathPoints (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowSightRays¶
-
CloseRangeVisibilityBuilder.
ShowSightRays
¶ Returns or sets the indication if blind volume sight rays will be displayed.
-------------------------------------
Getter Method
Signature
ShowSightRays
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowSightRays
Parameters: showSightRays (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
ShowTorsoLine¶
-
CloseRangeVisibilityBuilder.
ShowTorsoLine
¶ Returns or sets the indication if torso line will be displayed.
-------------------------------------
Getter Method
Signature
ShowTorsoLine
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ShowTorsoLine
Parameters: showTorsoLine (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Standard¶
-
CloseRangeVisibilityBuilder.
Standard
¶ Returns or sets the standard types to define the close range visibility.
-------------------------------------
Getter Method
Signature
Standard
Returns: Return type: str New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Standard
Parameters: standard (str) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
StepValue¶
-
CloseRangeVisibilityBuilder.
StepValue
¶ Returns or sets the step value to control the accurate for demo cylinder visibility and blind volume area calculation.
-------------------------------------
Getter Method
Signature
StepValue
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StepValue
Parameters: stepValue (float) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
UseMirror¶
-
CloseRangeVisibilityBuilder.
UseMirror
¶ Returns or sets the indication if the mirror will be used.
-------------------------------------
Getter Method
Signature
UseMirror
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseMirror
Parameters: useMirror (bool) – New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
VehicleBodies¶
-
CloseRangeVisibilityBuilder.
VehicleBodies
¶ Returns the bodies selection used to identify vehicle bodies.
-------------------------------------
Getter Method
Signature
VehicleBodies
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
VehicleFacetBodies¶
-
CloseRangeVisibilityBuilder.
VehicleFacetBodies
¶ Returns the bodies selection used to identify vehicle facet bodies.
-------------------------------------
Getter Method
Signature
VehicleFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
WindowFaces¶
-
CloseRangeVisibilityBuilder.
WindowFaces
¶ Returns the faces selection used to identify the vehicle window surfaces.
-------------------------------------
Getter Method
Signature
WindowFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
WindowFacetBodies¶
-
CloseRangeVisibilityBuilder.
WindowFacetBodies
¶ Returns the faces selection used to identify the vehicle window facet bodies.
-------------------------------------
Getter Method
Signature
WindowFacetBodies
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX11.0.0.
License requirements: None.
Method Detail¶
CreateCameraListItemBuilder¶
-
CloseRangeVisibilityBuilder.
CreateCameraListItemBuilder
¶ Creates a
NXOpen.Features.VehicleDesign.CloseRangeCameraListItemBuilder
Signature
CreateCameraListItemBuilder()
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeCameraListItemBuilder
New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
CreateDemoCylinderListItemBuilder¶
-
CloseRangeVisibilityBuilder.
CreateDemoCylinderListItemBuilder
¶ Creates a
NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilder
Signature
CreateDemoCylinderListItemBuilder()
Returns: Return type: NXOpen.Features.VehicleDesign.CloseRangeDemoCylinderListItemBuilder
New in version NX8.5.0.
License requirements: nx_general_packaging (“NX General Packaging”)
Validate¶
-
CloseRangeVisibilityBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.