CloseRangeVisibilityBuilderEyePointOffsetTypes Enumeration¶
NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilder.EyePointOffsetTypes is an alias for NXOpen.Features.VehicleDesign.CloseRangeVisibilityBuilderEyePointOffsetTypes
-
class
NXOpen.Features.VehicleDesign.
CloseRangeVisibilityBuilderEyePointOffsetTypes
¶ Bases:
object
This enum represents the eye position offset options.
Enum Members
Enum Member Enum Member Description NoOffset No offset AllOffsets All offsets ForwardOffset Forward offset SidewaysOffset Sideways offset UpwardOffset Upward offset -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-