UnsewBuilder Class¶
-
class
NXOpen.Features.
UnsewBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.Unsew
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateUnsewBuilder()
Default values.
Property Value KeepOriginal 0 ToolOption Face New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
EdgeCollector | Returns the edge collector |
FaceCollector | Returns the face collector |
KeepOriginal | Returns or sets the apply to copy of body option |
Output | Returns or sets the output body option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
ToolOption | Returns or sets the tool option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
UnsewBuilderUnsewOutput Enumeration | Unsew body option type. |
UnsewBuilderUnsewTool Enumeration | Unsew tool option type. |
Property Detail¶
EdgeCollector¶
-
UnsewBuilder.
EdgeCollector
¶ Returns the edge collector
-------------------------------------
Getter Method
Signature
EdgeCollector
Returns: Return type: NXOpen.ScCollector
New in version NX9.0.0.
License requirements: None.
FaceCollector¶
-
UnsewBuilder.
FaceCollector
¶ Returns the face collector
-------------------------------------
Getter Method
Signature
FaceCollector
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
KeepOriginal¶
-
UnsewBuilder.
KeepOriginal
¶ Returns or sets the apply to copy of body option
-------------------------------------
Getter Method
Signature
KeepOriginal
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KeepOriginal
Parameters: keepOriginal (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Output¶
-
UnsewBuilder.
Output
¶ Returns or sets the output body option
-------------------------------------
Getter Method
Signature
Output
Returns: Return type: NXOpen.Features.UnsewBuilderUnsewOutput
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Output
Parameters: output ( NXOpen.Features.UnsewBuilderUnsewOutput
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
ToolOption¶
-
UnsewBuilder.
ToolOption
¶ Returns or sets the tool option
-------------------------------------
Getter Method
Signature
ToolOption
Returns: Return type: NXOpen.Features.UnsewBuilderUnsewTool
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolOption
Parameters: toolOption ( NXOpen.Features.UnsewBuilderUnsewTool
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
UnsewBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.