UnsewBuilderUnsewTool Enumeration¶
NXOpen.Features.UnsewBuilder.UnsewTool is an alias for NXOpen.Features.UnsewBuilderUnsewTool
-
class
NXOpen.Features.
UnsewBuilderUnsewTool
¶ Bases:
object
Unsew tool option type.
Enum Members
Enum Member Enum Member Description Face selected faces to unsew Edge selected edges to split faces -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-