CornerCutBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
CornerCutBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Builder used to create or edit a
NXOpen.Features.ShipDesign.CornerCut
feature.To create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateCornerCutBuilder()
Default values.
Property Value DistanceTolerance 0.0254 (millimeters part), 0.001 (inches part) New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CornerList | Returns the list of corner points. |
CornerPoint | Returns or sets the corner point. |
DistanceTolerance | Returns or sets the distance tolerance. |
ManufacturingInformation | Returns the manufacturing stock builder that holds the manufacturing data. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PlacementFace | Returns the placement face from plate system to add corner cuts. |
PlacementType | Returns or sets the type of corner cut to create. |
PlateBodyCollector | Returns the collector containing the plate bodies that are to have corner cuts added. |
Spreadsheet | Returns the spreadsheet builder. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CornerCutBuilderCutOption Enumeration | Represents the corner cut option. |
Property Detail¶
CornerList¶
-
CornerCutBuilder.
CornerList
¶ Returns the list of corner points.
-------------------------------------
Getter Method
Signature
CornerList
Returns: Return type: NXOpen.Features.ShipDesign.CornerCutListItemBuilderList
New in version NX8.5.0.
License requirements: None.
CornerPoint¶
-
CornerCutBuilder.
CornerPoint
¶ Returns or sets the corner point.
-------------------------------------
Getter Method
Signature
CornerPoint
Returns: Return type: NXOpen.Point
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerPoint
Parameters: cornerPoint ( NXOpen.Point
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
DistanceTolerance¶
-
CornerCutBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance.
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ManufacturingInformation¶
-
CornerCutBuilder.
ManufacturingInformation
¶ Returns the manufacturing stock builder that holds the manufacturing data.
-------------------------------------
Getter Method
Signature
ManufacturingInformation
Returns: Return type: NXOpen.Features.ShipDesign.ManufacturingStockBuilder
New in version NX8.5.1.
License requirements: None.
PlacementFace¶
-
CornerCutBuilder.
PlacementFace
¶ Returns the placement face from plate system to add corner cuts.
-------------------------------------
Getter Method
Signature
PlacementFace
Returns: Return type: NXOpen.SelectTaggedObject
New in version NX12.0.0.
License requirements: None.
PlacementType¶
-
CornerCutBuilder.
PlacementType
¶ Returns or sets the type of corner cut to create.
-------------------------------------
Getter Method
Signature
PlacementType
Returns: Return type: NXOpen.Features.ShipDesign.CornerCutBuilderCutOption
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlacementType
Parameters: cutOption ( NXOpen.Features.ShipDesign.CornerCutBuilderCutOption
) –New in version NX8.5.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
PlateBodyCollector¶
-
CornerCutBuilder.
PlateBodyCollector
¶ Returns the collector containing the plate bodies that are to have corner cuts added.
-------------------------------------
Getter Method
Signature
PlateBodyCollector
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
Spreadsheet¶
-
CornerCutBuilder.
Spreadsheet
¶ Returns the spreadsheet builder.
Users can specify the Weldout using a single sketch. The sketch type and its parameters are controlled by the
NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
.-------------------------------------
Getter Method
Signature
Spreadsheet
Returns: Return type: NXOpen.Features.ShipDesign.SteelFeatureSpreadsheetBuilder
New in version NX8.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
CornerCutBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.