CornerCutBuilderCutOption Enumeration¶
NXOpen.Features.ShipDesign.CornerCutBuilder.CutOption is an alias for NXOpen.Features.ShipDesign.CornerCutBuilderCutOption
-
class
NXOpen.Features.ShipDesign.
CornerCutBuilderCutOption
¶ Bases:
object
Represents the corner cut option.
Enum Members
Enum Member Enum Member Description Corner Create corner cut on selected corner point. Plate Create corner cut for all corner points of the mold face of plate body -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-