TabBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
TabBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a Tab feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateTabFeatureBuilder()
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
IsSecondary | Returns or sets the tab type |
MaterialSide | Returns or sets the material side value of secondary tab |
MultiBendPropertiesList | Returns the multi bend properties list |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Section | Returns or sets the section of tab |
Sketch | Returns or sets the sketch of tab |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetBody | Returns or sets the target body on which the secondary tab is created. |
Thickness | Returns the thickness of tab |
ThicknessSide | Returns or sets the sweep direction flag of tab |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetThickness | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpdateReferenceCurves | This is only applicable for base tab created with bends. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify whether the builder data is valid for creating a Tab or not. |
Enumerations¶
TabBuilderSectionSideOptions Enumeration | This enum represents the side of the section that the dimple punches material. |
TabBuilderThicknessSideOptions Enumeration | This enum represents the extent direction for the Tab. |
Property Detail¶
IsSecondary¶
-
TabBuilder.
IsSecondary
¶ Returns or sets the tab type
-------------------------------------
Getter Method
Signature
IsSecondary
Returns: tab type Return type: bool New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
IsSecondary
Parameters: isSecondary (bool) – tab type New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
MaterialSide¶
-
TabBuilder.
MaterialSide
¶ Returns or sets the material side value of secondary tab
-------------------------------------
Getter Method
Signature
MaterialSide
Returns: material side value Return type: NXOpen.Features.SheetMetal.TabBuilderSectionSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
MaterialSide
Parameters: sectionSide ( NXOpen.Features.SheetMetal.TabBuilderSectionSideOptions
) – material side valueNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
MultiBendPropertiesList¶
-
TabBuilder.
MultiBendPropertiesList
¶ Returns the multi bend properties list
-------------------------------------
Getter Method
Signature
MultiBendPropertiesList
Returns: Return type: NXOpen.Features.SheetMetal.FeatureBendPropertiesListBuilder
New in version NX12.0.0.
License requirements: nx_flexible_pcb (“NX Flexible PCB”) OR nx_sheet_metal (“NX Sheet Metal”)
Section¶
-
TabBuilder.
Section
¶ Returns or sets the section of tab
-------------------------------------
Getter Method
Signature
Section
Returns: Section tag Return type: NXOpen.Section
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
Section
Parameters: section ( NXOpen.Section
) – section tagNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Sketch¶
-
TabBuilder.
Sketch
¶ Returns or sets the sketch of tab
-------------------------------------
Getter Method
Signature
Sketch
Returns: Sketch tag Return type: NXOpen.Features.SketchFeature
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
Sketch
Parameters: sketch ( NXOpen.Features.SketchFeature
) – sketch tagNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
TargetBody¶
-
TabBuilder.
TargetBody
¶ Returns or sets the target body on which the secondary tab is created.
Use
NXOpen.Features.SheetMetal.TabBuilder.IsSecondary()
to determine whether this is a secondary tab.-------------------------------------
Getter Method
Signature
TargetBody
Returns: Returns the target body on which the secondary tab is created. Return type: NXOpen.Body
New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
TargetBody
Parameters: targetBody ( NXOpen.Body
) – A sheet metal body on which secondary tab is to be created.New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Thickness¶
-
TabBuilder.
Thickness
¶ Returns the thickness of tab
-------------------------------------
Getter Method
Signature
Thickness
Returns: Tab thickness Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ThicknessSide¶
-
TabBuilder.
ThicknessSide
¶ Returns or sets the sweep direction flag of tab
-------------------------------------
Getter Method
Signature
ThicknessSide
Returns: Sweep Direction Flag Return type: NXOpen.Features.SheetMetal.TabBuilderThicknessSideOptions
New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
ThicknessSide
Parameters: flag ( NXOpen.Features.SheetMetal.TabBuilderThicknessSideOptions
) – Sweep Direction FlagNew in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
SetThickness¶
-
TabBuilder.
SetThickness
¶ Signature
SetThickness(thickness)
Parameters: thickness (str) – Tab thickness New in version NX4.0.0.
Deprecated since version NX10.0.0: Use
NXOpen.Expression.RightHandSide()
on theNXOpen.Expression
object returned fromNXOpen.Features.SheetMetal.TabBuilder.Thickness()
instead.License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
UpdateReferenceCurves¶
-
TabBuilder.
UpdateReferenceCurves
¶ This is only applicable for base tab created with bends.
This extracts boundary curves of the faces that are attached to the planes specified by
NXOpen.Features.SheetMetal.MultiBendBendPropertiesBuilder.Plane`()
.Signature
UpdateReferenceCurves()
Returns: Return type: NXOpen.Features.Feature
New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Validate¶
-
TabBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
TabBuilder.
ValidateBuilderData
¶ Verify whether the builder data is valid for creating a Tab or not.
If the Builder data is valid, returned value shall be 0.
Signature
ValidateBuilderData()
Returns: Data Validity Flag. Return type: int New in version NX4.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)