FeatureBendPropertiesListBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
FeatureBendPropertiesListBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalComponentBuilder
Represents a Sheetmetal Feature properties List builder class.
This builder is used to interrogate the feature properties list. .. versionadded:: NX12.0.0
Properties¶
Property | Description |
---|---|
FeatureBendPropertiesList | Returns the feature properties list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateFeatureProperties | Create a feature properties. |
GetApplicationContext | Get the application context. |
SetApplicationContext | Set the application context. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FeatureBendPropertiesList¶
-
FeatureBendPropertiesListBuilder.
FeatureBendPropertiesList
¶ Returns the feature properties list
-------------------------------------
Getter Method
Signature
FeatureBendPropertiesList
Returns: Return type: NXOpen.Features.SheetMetal.FeatureBendPropertiesBuilderList
New in version NX12.0.0.
License requirements: None.
Method Detail¶
CreateFeatureProperties¶
-
FeatureBendPropertiesListBuilder.
CreateFeatureProperties
¶ Create a feature properties.
Signature
CreateFeatureProperties()
Returns: Return type: NXOpen.Features.SheetMetal.FeatureBendPropertiesBuilder
New in version NX12.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”) OR nx_ship_detail (“Ship Detail Design”)
Validate¶
-
FeatureBendPropertiesListBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.