FeatureBendPropertiesBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
FeatureBendPropertiesBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalComponentBuilder
Represents a Sheetmetal Feature bend properties builder class.
This builder is used to interrogate the feature properties in the list. To create a new instance of this class, use
NXOpen.Features.SheetMetal.FeatureBendPropertiesListBuilder.CreateFeatureProperties()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
BendOptions | Returns the Sheet Metal Bend Options |
Tag | Returns the Tag for this object. |
Value | Returns the offset |
Methods¶
Method | Description |
---|---|
GetApplicationContext | Get the application context. |
SetApplicationContext | Set the application context. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BendOptions¶
-
FeatureBendPropertiesBuilder.
BendOptions
¶ Returns the Sheet Metal Bend Options
-------------------------------------
Getter Method
Signature
BendOptions
Returns: Return type: NXOpen.Features.SheetMetal.BendOptions
New in version NX12.0.0.
License requirements: None.
Value¶
-
FeatureBendPropertiesBuilder.
Value
¶ Returns the offset
-------------------------------------
Getter Method
Signature
Value
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
FeatureBendPropertiesBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.