BendBuilder Class¶
-
class
NXOpen.Features.SheetMetal.
BendBuilder
¶ Bases:
NXOpen.Features.SheetMetal.SheetmetalBaseBuilder
Represents a Bend feature builder.
To create a new instance of this class, use
NXOpen.Features.SheetMetal.SheetmetalManager.CreateBendFeatureBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BendLocation | Returns or sets the Bend Location (Material Side) |
BendOptions | Returns the Bend Options. |
Direction | Returns or sets the Bend Direction |
ExtendProfile | Returns or sets the Extend Option |
FixedSide | Returns or sets the Fixed Side |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Section | Returns or sets the Section |
Sketch | Returns or sets the Sketch |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TargetFace | Returns or sets the target face on which bend feature applies. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetApplicationContext | Get the application context. |
GetBendAngle | Returns the Bend Angle |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetApplicationContext | Set the application context. |
SetBendAngle | Sets the Bend Angle |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
ValidateBuilderData | Verify whether the builder data is valid for creating bend or not. |
Enumerations¶
BendBuilderBendDirectionOptions Enumeration | This enum represents the Bend Direction for Bend. |
BendBuilderBendLocationOptions Enumeration | This enum represents the Bend Location (Material Side) for Bend. |
BendBuilderFixedSideOptions Enumeration | This enum represents the Fixed Side for Bend. |
Property Detail¶
BendLocation¶
-
BendBuilder.
BendLocation
¶ Returns or sets the Bend Location (Material Side)
-------------------------------------
Getter Method
Signature
BendLocation
Returns: Return type: NXOpen.Features.SheetMetal.BendBuilderBendLocationOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
BendLocation
Parameters: bendLocation ( NXOpen.Features.SheetMetal.BendBuilderBendLocationOptions
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
BendOptions¶
-
BendBuilder.
BendOptions
¶ Returns the Bend Options.
The option
Features.SheetMetal.BendOptionsCornerReliefTypeOptions.None
is not valid for theFeatures.Bend
starting NX11 onwards.From NX 12
Features.SheetMetal.BendOptions.ExtendBendRelief()
has no effect on the Bend feature.-------------------------------------
Getter Method
Signature
BendOptions
Returns: Return type: NXOpen.Features.SheetMetal.BendOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Direction¶
-
BendBuilder.
Direction
¶ Returns or sets the Bend Direction
-------------------------------------
Getter Method
Signature
Direction
Returns: Return type: NXOpen.Features.SheetMetal.BendBuilderBendDirectionOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
Direction
Parameters: direction ( NXOpen.Features.SheetMetal.BendBuilderBendDirectionOptions
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
ExtendProfile¶
-
BendBuilder.
ExtendProfile
¶ Returns or sets the Extend Option
-------------------------------------
Getter Method
Signature
ExtendProfile
Returns: Return type: bool New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
ExtendProfile
Parameters: extendOption (bool) – New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
FixedSide¶
-
BendBuilder.
FixedSide
¶ Returns or sets the Fixed Side
-------------------------------------
Getter Method
Signature
FixedSide
Returns: Return type: NXOpen.Features.SheetMetal.BendBuilderFixedSideOptions
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
FixedSide
Parameters: fixedSide ( NXOpen.Features.SheetMetal.BendBuilderFixedSideOptions
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Section¶
-
BendBuilder.
Section
¶ Returns or sets the Section
-------------------------------------
Getter Method
Signature
Section
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
Section
Parameters: section ( NXOpen.Section
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Sketch¶
-
BendBuilder.
Sketch
¶ Returns or sets the Sketch
-------------------------------------
Getter Method
Signature
Sketch
Returns: Return type: NXOpen.Features.SketchFeature
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
Sketch
Parameters: sketch ( NXOpen.Features.SketchFeature
) –New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
TargetFace¶
-
BendBuilder.
TargetFace
¶ Returns or sets the target face on which bend feature applies.
-------------------------------------
Getter Method
Signature
TargetFace
Returns: Returns the target face on which the bend feature is created. Return type: NXOpen.Face
New in version NX10.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
-------------------------------------
Setter Method
Signature
TargetFace
Parameters: targetFace ( NXOpen.Face
) – A planar non-deform sheet metal face on which the bend feature is to be created.New in version NX10.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Method Detail¶
GetBendAngle¶
-
BendBuilder.
GetBendAngle
¶ Returns the Bend Angle
Signature
GetBendAngle()
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
SetBendAngle¶
-
BendBuilder.
SetBendAngle
¶ Sets the Bend Angle
Signature
SetBendAngle(bendAngle)
Parameters: bendAngle (str) – New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)
Validate¶
-
BendBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.
ValidateBuilderData¶
-
BendBuilder.
ValidateBuilderData
¶ Verify whether the builder data is valid for creating bend or not.
If the Builder data is valid, returned value should be 0
Signature
ValidateBuilderData()
Returns: Data Validity Flag. Return type: int New in version NX5.0.0.
License requirements: nx_sheet_metal (“NX Sheet Metal”) OR nx_flexible_pcb (“NX Flexible PCB”)