BendBuilderBendDirectionOptions Enumeration

NXOpen.Features.SheetMetal.BendBuilder.BendDirectionOptions is an alias for NXOpen.Features.SheetMetal.BendBuilderBendDirectionOptions

class NXOpen.Features.SheetMetal.BendBuilderBendDirectionOptions

Bases: object

This enum represents the Bend Direction for Bend.

New in version NX5.0.0.

Enum Members

Enum Member Enum Member Description
SectionNormalSide Bend is created on the side of the section normal.
SectionReverseNormalSide Bend is created on the side opposite to that of the section normal
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.