ReplaceFaceBuilder Class¶
-
class
NXOpen.Features.
ReplaceFaceBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder for a replace face feature, don’t use it until nx502.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateReplaceFaceBuilder()
New in version NX5.0.2.
Properties¶
Property | Description |
---|---|
BlendFace | Returns the face collector holding the all the recognized blend faces adjacent to faces to replace. |
FaceChangeOverflowBehavior | Returns the face change overflow behavior. |
FaceToReplace | Returns the target faces to replace, only for replace type, don’t use it until nx502 |
FaceToSimplify | Returns the face to simplify, only for simplify type, don’t use it until nx502 |
FreeEdgeProjection | Returns the free edge projection options, which defines a direction to project laminar boundaries of the original face onto the replacement face. |
OffsetDistance | Returns the offset distance of replacement faces |
OffsetReverseDirection | Returns or sets the offset reverse direction flag of replacement faces |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ReplaceFaces | Returns the target faces to replace |
ReplacementFace | Returns the replacement face, only for replace type, don’t use it until nx502 |
ReplacementFaces | Returns the replacement faces |
ReverseDirection | Returns or sets the flag of reverse direction between replace face and the surface of replacement face, only for replace type, don’t use it until nx502 |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the replace face type, don’t use it until further notification |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
ResetFreeEdgeProjectionOption | The function used to set m_resetFreeEdgeProjectionOption in ReplaceFaceBuilder as true |
ResetReplaceFaceMethod | The function used to set m_resetReplaceFaceMethod in ReplaceFaceBuilder as true |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ReplaceFaceBuilderReplaceTypes Enumeration | Enumeration of replace face type, don’t use it until nx502 |
Property Detail¶
BlendFace¶
-
ReplaceFaceBuilder.
BlendFace
¶ Returns the face collector holding the all the recognized blend faces adjacent to faces to replace.
It is auto recognized blends + user selected blends - user excluded blends, don’t use it until nx502
-------------------------------------
Getter Method
Signature
BlendFace
Returns: Return type: NXOpen.ModlDirect.SelectBlend
New in version NX5.0.2.
License requirements: None.
FaceChangeOverflowBehavior¶
-
ReplaceFaceBuilder.
FaceChangeOverflowBehavior
¶ Returns the face change overflow behavior.
Please refer
NXOpen.GeometricUtilities.FaceChangeOverflowBehavior
for details.-------------------------------------
Getter Method
Signature
FaceChangeOverflowBehavior
Returns: Return type: NXOpen.GeometricUtilities.FaceChangeOverflowBehavior
New in version NX6.0.2.
License requirements: None.
FaceToReplace¶
-
ReplaceFaceBuilder.
FaceToReplace
¶ Returns the target faces to replace, only for replace type, don’t use it until nx502
-------------------------------------
Getter Method
Signature
FaceToReplace
Returns: the replace faces collector Return type: NXOpen.ScCollector
New in version NX5.0.2.
License requirements: None.
FaceToSimplify¶
-
ReplaceFaceBuilder.
FaceToSimplify
¶ Returns the face to simplify, only for simplify type, don’t use it until nx502
-------------------------------------
Getter Method
Signature
FaceToSimplify
Returns: the list of faces to simplify Return type: NXOpen.SelectFaceList
New in version NX5.0.2.
License requirements: None.
FreeEdgeProjection¶
-
ReplaceFaceBuilder.
FreeEdgeProjection
¶ Returns the free edge projection options, which defines a direction to project laminar boundaries of the original face onto the replacement face.
-------------------------------------
Getter Method
Signature
FreeEdgeProjection
Returns: Return type: NXOpen.GeometricUtilities.ProjectionOptions
New in version NX11.0.0.
License requirements: None.
OffsetDistance¶
-
ReplaceFaceBuilder.
OffsetDistance
¶ Returns the offset distance of replacement faces
-------------------------------------
Getter Method
Signature
OffsetDistance
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
OffsetReverseDirection¶
-
ReplaceFaceBuilder.
OffsetReverseDirection
¶ Returns or sets the offset reverse direction flag of replacement faces
-------------------------------------
Getter Method
Signature
OffsetReverseDirection
Returns: the flag of offset reverse direction Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OffsetReverseDirection
Parameters: reverseDirection (bool) – the flag of offset reverse direction New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
ReplaceFaces¶
-
ReplaceFaceBuilder.
ReplaceFaces
¶ Returns the target faces to replace
-------------------------------------
Getter Method
Signature
ReplaceFaces
Returns: the replace faces collector Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
ReplacementFace¶
-
ReplaceFaceBuilder.
ReplacementFace
¶ Returns the replacement face, only for replace type, don’t use it until nx502
-------------------------------------
Getter Method
Signature
ReplacementFace
Returns: the replacement faces collector Return type: NXOpen.SelectFace
New in version NX5.0.2.
License requirements: None.
ReplacementFaces¶
-
ReplaceFaceBuilder.
ReplacementFaces
¶ Returns the replacement faces
-------------------------------------
Getter Method
Signature
ReplacementFaces
Returns: the replacement faces collector Return type: NXOpen.ScCollector
New in version NX6.0.0.
License requirements: None.
ReverseDirection¶
-
ReplaceFaceBuilder.
ReverseDirection
¶ Returns or sets the flag of reverse direction between replace face and the surface of replacement face, only for replace type, don’t use it until nx502
-------------------------------------
Getter Method
Signature
ReverseDirection
Returns: the flag of reverse direction or not Return type: bool New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection
Parameters: reverseDirection (bool) – the flag of reverse direction or not New in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Type¶
-
ReplaceFaceBuilder.
Type
¶ Returns or sets the replace face type, don’t use it until further notification
-------------------------------------
Getter Method
Signature
Type
Returns: the replace face type Return type: NXOpen.Features.ReplaceFaceBuilderReplaceTypes
New in version NX5.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: replaceType ( NXOpen.Features.ReplaceFaceBuilderReplaceTypes
) – the replace face typeNew in version NX5.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
ResetFreeEdgeProjectionOption¶
-
ReplaceFaceBuilder.
ResetFreeEdgeProjectionOption
¶ The function used to set m_resetFreeEdgeProjectionOption in ReplaceFaceBuilder as true
Signature
ResetFreeEdgeProjectionOption()
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
ResetReplaceFaceMethod¶
-
ReplaceFaceBuilder.
ResetReplaceFaceMethod
¶ The function used to set m_resetReplaceFaceMethod in ReplaceFaceBuilder as true
Signature
ResetReplaceFaceMethod()
New in version NX10.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”)
Validate¶
-
ReplaceFaceBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.