FaceChangeOverflowBehavior Class¶
-
class
NXOpen.GeometricUtilities.
FaceChangeOverflowBehavior
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.GeometricUtilities.FaceChangeOverflowBehavior
It provides several face change options for controlling behavior when a change face overflows an incident face.New in version NX6.0.2.
Properties¶
Property | Description |
---|---|
FaceChangeOption | Returns or sets the face change option. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
FaceChangeOverflowBehaviorOption Enumeration | face change option. |
Property Detail¶
FaceChangeOption¶
-
FaceChangeOverflowBehavior.
FaceChangeOption
¶ Returns or sets the face change option.
-------------------------------------
Getter Method
Signature
FaceChangeOption
Returns: Return type: NXOpen.GeometricUtilities.FaceChangeOverflowBehaviorOption
New in version NX6.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceChangeOption
Parameters: faceChangeOption ( NXOpen.GeometricUtilities.FaceChangeOverflowBehaviorOption
) –New in version NX6.0.2.
License requirements: solid_modeling (“SOLIDS MODELING”) OR cam_base (“CAM BASE”) OR insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
Validate¶
-
FaceChangeOverflowBehavior.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.