RPOBuilder Class¶
-
class
NXOpen.Features.
RPOBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a RPO builder.
It provides methods to create positioning dimensions to position the feature which is being created.
This is an abstract class, and cannot be instantiated
New in version NX3.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
ApplyDimensions | Transforms the feature by applying the positioning dimensions |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreateDimension | Creates a new empty RPODimension object |
CreatePositioningDimension | Creates a positioning dimension. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetReferenceDirection | Query/Set a horizontal or vertical reference for the feature. |
GetRpoDimensions | Gets the list of RPO dimemsions |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
HidePositioningDimensions | Hides display of all the positioning dimensions |
SetExpression | Sets the expression value in order to constrain the target and tool entities which are set using NXOpen.Features.RPOBuilder.SetTargetAndTool() . |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetReferenceDirection | Sets a horizontal or vertical reference for the feature. |
SetRpoDimensions | Sets the list of RPO dimemsions |
SetTargetAndTool | Sets the target and tool entities. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowPositioningDimensions | Displays all the positioning dimensions |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UndoLastDimension | Undo the last positioning dimension |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RPOBuilderAssociativityType Enumeration | Represents the associativity type for a dimension entity |
Method Detail¶
ApplyDimensions¶
-
RPOBuilder.
ApplyDimensions
¶ Transforms the feature by applying the positioning dimensions
Signature
ApplyDimensions()
New in version NX3.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
CreateDimension¶
-
RPOBuilder.
CreateDimension
¶ Creates a new empty RPODimension object
Signature
CreateDimension()
Returns: The RPO dimensions Return type: NXOpen.Features.RPODimension
New in version NX4.0.0.
License requirements: None.
CreatePositioningDimension¶
-
RPOBuilder.
CreatePositioningDimension
¶ Creates a positioning dimension.
This is third and the last step in creating a positioning dimension.
Signature
CreatePositioningDimension()
New in version NX3.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
GetReferenceDirection¶
-
RPOBuilder.
GetReferenceDirection
¶ Query/Set a horizontal or vertical reference for the feature.
A reference is required to be set before creating a Horizontal or Vertical positioning dimension.
Signature
GetReferenceDirection()
Returns: a tuple Return type: A tuple consisting of (reference, orientation). reference is a NXOpen.IReferenceAxis
. Reference entity orientation is aNXOpen.AxisOrientation
. Orientation of referenceNew in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
GetRpoDimensions¶
-
RPOBuilder.
GetRpoDimensions
¶ Gets the list of RPO dimemsions
Signature
GetRpoDimensions()
Returns: The RPO dimensions Return type: list of NXOpen.Features.RPODimension
New in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
HidePositioningDimensions¶
-
RPOBuilder.
HidePositioningDimensions
¶ Hides display of all the positioning dimensions
Signature
HidePositioningDimensions()
New in version NX3.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
SetExpression¶
-
RPOBuilder.
SetExpression
¶ Sets the expression value in order to constrain the target and tool entities which are set using
NXOpen.Features.RPOBuilder.SetTargetAndTool()
.This is the second step in creating a positioning dimension. This step is not needed for
NXOpen.PositioningDimensionSubtype.PointOntoPoint
,NXOpen.PositioningDimensionSubtype.PointOntoLine
andNXOpen.PositioningDimensionSubtype.LineOntoLine
Signature
SetExpression(expression)
Parameters: expression (str) – Expression string New in version NX3.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
SetReferenceDirection¶
-
RPOBuilder.
SetReferenceDirection
¶ Sets a horizontal or vertical reference for the feature.
A reference is required to be set before creating a
NXOpen.PositioningDimensionSubtype.Horizontal
orNXOpen.PositioningDimensionSubtype.Vertical
subtype of positioning dimension.Signature
SetReferenceDirection(reference, orientation)
Parameters: - reference (
NXOpen.IReferenceAxis
) – Reference entity - orientation (
NXOpen.AxisOrientation
) – Orientation of reference
New in version NX3.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
- reference (
SetRpoDimensions¶
-
RPOBuilder.
SetRpoDimensions
¶ Sets the list of RPO dimemsions
Signature
SetRpoDimensions(dimensions)
Parameters: dimensions (list of NXOpen.Features.RPODimension
) – The RPO dimensionsNew in version NX4.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
SetTargetAndTool¶
-
RPOBuilder.
SetTargetAndTool
¶ Sets the target and tool entities.
This is the first step in creating a positioning dimension. A positioning dimension constraints two entities. These two entities are referred to as target and tool enitities. The tool entity is selected from the tool body which is being created. For example, if a Pad is being created then the tool entity can be an edge of the Pad. The target entity is an entity which does not belong to the tool body which is being created.
Signature
SetTargetAndTool(subtype, target, targetAssociativity, targetHelpPoint, tool, toolAssociativity, toolHelpPoint)
Parameters: - subtype (
NXOpen.PositioningDimensionSubtype
) – Subtype of dimension - target (
NXOpen.NXObject
) – Target entity - targetAssociativity (
NXOpen.Features.RPOBuilderAssociativityType
) – Associativity for target entity - targetHelpPoint (
NXOpen.Point3d
) – Help point for taregt entity - tool (
NXOpen.NXObject
) – Tool entity - toolAssociativity (
NXOpen.Features.RPOBuilderAssociativityType
) – Associativity for tool entity - toolHelpPoint (
NXOpen.Point3d
) – Help point for tool entity
New in version NX3.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
- subtype (
ShowPositioningDimensions¶
-
RPOBuilder.
ShowPositioningDimensions
¶ Displays all the positioning dimensions
Signature
ShowPositioningDimensions()
New in version NX3.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
UndoLastDimension¶
-
RPOBuilder.
UndoLastDimension
¶ Undo the last positioning dimension
Signature
UndoLastDimension()
New in version NX3.0.0.
License requirements: features_modeling (“FEATURES MODELING”), solid_modeling (“SOLIDS MODELING”)
Validate¶
-
RPOBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.