PositioningDimensionSubtype Enumeration¶
NXOpen.PositioningDimension.Subtype is an alias for NXOpen.PositioningDimensionSubtype
-
class
NXOpen.
PositioningDimensionSubtype
¶ Bases:
object
Represents the subtype of the positioning dimension
Enum Members
Enum Member Enum Member Description Horizontal Horizontal dimension Vertical Vertical dimension Parallel Parallel dimension Perpendicular Perpendicular dimension ParallelDistance Parallel at a distance dimension Angular Angular dimension PointOntoPoint Point onto point dimension PointOntoLine Point onto line dimension LineOntoLine Line onto line dimension -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-