JoeBuilder Class¶
-
class
NXOpen.Features.
JoeBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Builds a Joe feature
To create a new instance of this class, use
NXOpen.DebugSession.CreateJoeBuilder()
Default values.
Property Value LineWidthTest.LineWidthSettings.Width Normal LineWidthTest.LineWidthSettings.WidthOption Assigned Toggle False ValueTest.Color 5 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
AngularDimension | Returns the angular dimension |
BooleanOperation | Returns the boolean operation |
DateTest | Returns the date and time |
Dimension | Returns the length |
DisableSelections | Returns or sets the flag that if true, section, selection, and other selections are disabled |
DiscreetType | Returns or sets the discreet type |
DoubleLinearDimension | Returns the double linear dimension |
EnumTest | Returns the enum test |
Expression | Returns the expression |
Integer | Returns or sets the integer |
LineWidthTest | Returns the line width |
List | Returns the list |
Name | Returns or sets the name |
OnPathDim | Returns |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Path | Returns |
Point | Returns or sets the location |
RadiusDimension | Returns the radius dimension |
Section | Returns the section |
Seldimlist | Returns the seldimlist |
Selection | Returns the selected object |
StringTest | Returns the string test |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Toggle | Returns or sets the toggle |
Tolerance | Returns or sets the tolerance |
TwoSidedAngular | Returns the two-sided angular dimension |
TwoSidedLinear | Returns the two-sided linear dimension |
ValueTest | Returns the value test |
Methods¶
Method | Description |
---|---|
ActionButton | Do an action |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DoSevereException | Tests doing a severe exception |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetLines | The lines of text |
GetNonItiLines | Non-iti lines of text |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
NewListItem | Creates a new list item |
SetLines | |
SetNonItiLines | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
JoeBuilderDiscreetTypes Enumeration | Enumeration of discreet types |
Property Detail¶
AngularDimension¶
-
JoeBuilder.
AngularDimension
¶ Returns the angular dimension
-------------------------------------
Getter Method
Signature
AngularDimension
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
BooleanOperation¶
-
JoeBuilder.
BooleanOperation
¶ Returns the boolean operation
-------------------------------------
Getter Method
Signature
BooleanOperation
Returns: Return type: NXOpen.GeometricUtilities.BooleanOperation
New in version NX5.0.0.
License requirements: None.
DateTest¶
-
JoeBuilder.
DateTest
¶ Returns the date and time
-------------------------------------
Getter Method
Signature
DateTest
Returns: Return type: NXOpen.DateTest
New in version NX8.0.0.
License requirements: None.
Dimension¶
-
JoeBuilder.
Dimension
¶ Returns the length
-------------------------------------
Getter Method
Signature
Dimension
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
DisableSelections¶
-
JoeBuilder.
DisableSelections
¶ Returns or sets the flag that if true, section, selection, and other selections are disabled
-------------------------------------
Getter Method
Signature
DisableSelections
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisableSelections
Parameters: disableSelections (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DiscreetType¶
-
JoeBuilder.
DiscreetType
¶ Returns or sets the discreet type
-------------------------------------
Getter Method
Signature
DiscreetType
Returns: Return type: NXOpen.Features.JoeBuilderDiscreetTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DiscreetType
Parameters: discreetType ( NXOpen.Features.JoeBuilderDiscreetTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DoubleLinearDimension¶
-
JoeBuilder.
DoubleLinearDimension
¶ Returns the double linear dimension
-------------------------------------
Getter Method
Signature
DoubleLinearDimension
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
EnumTest¶
-
JoeBuilder.
EnumTest
¶ Returns the enum test
-------------------------------------
Getter Method
Signature
EnumTest
Returns: Return type: NXOpen.GeometricUtilities.EnumTest
New in version NX5.0.0.
License requirements: None.
Expression¶
-
JoeBuilder.
Expression
¶ Returns the expression
-------------------------------------
Getter Method
Signature
Expression
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Integer¶
-
JoeBuilder.
Integer
¶ Returns or sets the integer
-------------------------------------
Getter Method
Signature
Integer
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Integer
Parameters: integer (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
LineWidthTest¶
-
JoeBuilder.
LineWidthTest
¶ Returns the line width
-------------------------------------
Getter Method
Signature
LineWidthTest
Returns: Return type: NXOpen.LineWidthTestBuilder
New in version NX8.0.0.
License requirements: None.
List¶
-
JoeBuilder.
List
¶ Returns the list
-------------------------------------
Getter Method
Signature
List
Returns: Return type: NXOpen.Features.JoeListItemList
New in version NX5.0.0.
License requirements: None.
Name¶
-
JoeBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
OnPathDim¶
-
JoeBuilder.
OnPathDim
¶ Returns
-------------------------------------
Getter Method
Signature
OnPathDim
Returns: Return type: NXOpen.GeometricUtilities.OnPathDimensionBuilder
New in version NX5.0.0.
License requirements: None.
Path¶
-
JoeBuilder.
Path
¶ Returns
-------------------------------------
Getter Method
Signature
Path
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
Point¶
-
JoeBuilder.
Point
¶ Returns or sets the location
-------------------------------------
Getter Method
Signature
Point
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point
Parameters: location ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RadiusDimension¶
-
JoeBuilder.
RadiusDimension
¶ Returns the radius dimension
-------------------------------------
Getter Method
Signature
RadiusDimension
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
Section¶
-
JoeBuilder.
Section
¶ Returns the section
-------------------------------------
Getter Method
Signature
Section
Returns: Return type: NXOpen.Section
New in version NX5.0.0.
License requirements: None.
Seldimlist¶
-
JoeBuilder.
Seldimlist
¶ Returns the seldimlist
-------------------------------------
Getter Method
Signature
Seldimlist
Returns: Return type: NXOpen.ExpressionCollectorSetList
New in version NX5.0.0.
License requirements: None.
Selection¶
-
JoeBuilder.
Selection
¶ Returns the selected object
-------------------------------------
Getter Method
Signature
Selection
Returns: Return type: NXOpen.SelectObjectList
New in version NX5.0.0.
License requirements: None.
StringTest¶
-
JoeBuilder.
StringTest
¶ Returns the string test
-------------------------------------
Getter Method
Signature
StringTest
Returns: Return type: NXOpen.GeometricUtilities.StringTestBuilder
New in version NX5.0.0.
License requirements: None.
Toggle¶
-
JoeBuilder.
Toggle
¶ Returns or sets the toggle
-------------------------------------
Getter Method
Signature
Toggle
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Toggle
Parameters: convex (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Tolerance¶
-
JoeBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
TwoSidedAngular¶
-
JoeBuilder.
TwoSidedAngular
¶ Returns the two-sided angular dimension
-------------------------------------
Getter Method
Signature
TwoSidedAngular
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
TwoSidedLinear¶
-
JoeBuilder.
TwoSidedLinear
¶ Returns the two-sided linear dimension
-------------------------------------
Getter Method
Signature
TwoSidedLinear
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
ValueTest¶
-
JoeBuilder.
ValueTest
¶ Returns the value test
-------------------------------------
Getter Method
Signature
ValueTest
Returns: Return type: NXOpen.GeometricUtilities.ValueTestBuilder
New in version NX5.0.0.
License requirements: None.
Method Detail¶
ActionButton¶
-
JoeBuilder.
ActionButton
¶ Do an action
Signature
ActionButton()
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DoSevereException¶
-
JoeBuilder.
DoSevereException
¶ Tests doing a severe exception
Signature
DoSevereException()
New in version NX6.0.1.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetLines¶
-
JoeBuilder.
GetLines
¶ The lines of text
Signature
GetLines()
Returns: Return type: list of str New in version NX5.0.0.
License requirements: None.
GetNonItiLines¶
-
JoeBuilder.
GetNonItiLines
¶ Non-iti lines of text
Signature
GetNonItiLines()
Returns: Return type: list of str New in version NX5.0.0.
License requirements: None.
NewListItem¶
-
JoeBuilder.
NewListItem
¶ Creates a new list item
Signature
NewListItem(value, name, position)
Parameters: - value (float) – initial value in part units
- name (str) – name
- position (int) – position
Returns: Return type: New in version NX5.0.0.
License requirements: None.
SetLines¶
-
JoeBuilder.
SetLines
¶ Signature
SetLines(lines)
Parameters: lines (list of str) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetNonItiLines¶
-
JoeBuilder.
SetNonItiLines
¶ Signature
SetNonItiLines(lines)
Parameters: lines (list of str) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
JoeBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.