JoeBuilderDiscreetTypes Enumeration

NXOpen.Features.JoeBuilder.DiscreetTypes is an alias for NXOpen.Features.JoeBuilderDiscreetTypes

class NXOpen.Features.JoeBuilderDiscreetTypes

Bases: object

Enumeration of discreet types

New in version NX5.0.0.

Enum Members

Enum Member Enum Member Description
Option1
Option2
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.