IFormBuilder Class¶
-
class
NXOpen.Features.
IFormBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.IForm
builder.This class allows definition of iso-parameter curves on a face. These curves then can be shaped using
NXOpen.GeometricUtilities.CurveShapingBuilder
to finally shape the face.To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateIformBuilder()
Default values.
Property Value BSurfaceExtractionOption Original CanApplyToAll 0 CanKeepParameterization 0 CurveShaper.HasLinearTransition false CurveShaper.InsertionMethod Uniform CurveShaper.MovementMethod Normal CurveShaper.Number 1 CurveShaper.WCSOption XY FaceToDeform.CoaxialEnabled 0 FaceToDeform.CoplanarAxesEnabled 0 FaceToDeform.CoplanarEnabled 0 FaceToDeform.EqualDiameterEnabled 0 FaceToDeform.OffsetEnabled 0 FaceToDeform.ParallelEnabled 0 FaceToDeform.PerpendicularEnabled 0 FaceToDeform.SymmetricEnabled 0 FaceToDeform.TangentEnabled 0 FaceToDeform.ThicknessChainEnabled 0 FaceToDeform.UseFaceBrowse 1 InsertionMethod Uniform Number 3 ParameterDirection IsoU TransitionType Global UMaxContinuity.ContinuityType G0 UMinContinuity.ContinuityType G0 VMaxContinuity.ContinuityType G0 VMinContinuity.ContinuityType G0 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
BSurfaceExtractionOption | Returns or sets the b-surface extraction option |
CanApplyToAll | Returns or sets the value indicating if continuity is to be applied to all sides of the surface |
CanCreateNewBody | Returns or sets whether the operation is applied to a copy of the face there by creating new body |
CanKeepParameterization | Returns or sets the value indicating if input surface parameterization should be preserved during deformation |
CurveShaper | Returns the iso-parameter curve shaper |
ExtractTolerance | Returns or sets the tolerance used for b-surface extraction from a face |
FaceToDeform | Returns the face to deform. |
InsertionMethod | Returns or sets the iso-parameter curve insertion method |
Number | Returns or sets the number of iso-parameter curves to be inserted |
ParameterDirection | Returns or sets the iso-parameter direction |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SpecifyPoints | Returns the specified points to define iso-parameter curve |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
TransitionType | Returns or sets the transition options for local surface deformation |
UMaxContinuity | Returns the continuity at maximum U direction |
UMinContinuity | Returns the continuity at minimum U direction |
VMaxContinuity | Returns the continuity at maximum U direction |
VMinContinuity | Returns the continuity at minimum V direction |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
DeleteCurve | Deletes a iso-parameter curve |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
RemoveFeatureParameters | Removes parameters of a owning feature of a face to be deformed |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
IFormBuilderBSurfaceExtractionOptions Enumeration | B-surface extraction options |
IFormBuilderGlobalTransitionTypes Enumeration | Global transition options of the surface |
IFormBuilderInsertionMethodOptions Enumeration | Iso-parameter curve insertion option |
IFormBuilderParameterDirectionOptions Enumeration | Iso-parameter direction options |
IFormBuilderTransitionTypes Enumeration | Transition options of the surface |
Property Detail¶
BSurfaceExtractionOption¶
-
IFormBuilder.
BSurfaceExtractionOption
¶ Returns or sets the b-surface extraction option
-------------------------------------
Getter Method
Signature
BSurfaceExtractionOption
Returns: Return type: NXOpen.Features.IFormBuilderBSurfaceExtractionOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BSurfaceExtractionOption
Parameters: option ( NXOpen.Features.IFormBuilderBSurfaceExtractionOptions
) –New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CanApplyToAll¶
-
IFormBuilder.
CanApplyToAll
¶ Returns or sets the value indicating if continuity is to be applied to all sides of the surface
-------------------------------------
Getter Method
Signature
CanApplyToAll
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanApplyToAll
Parameters: applyToAll (bool) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CanCreateNewBody¶
-
IFormBuilder.
CanCreateNewBody
¶ Returns or sets whether the operation is applied to a copy of the face there by creating new body
-------------------------------------
Getter Method
Signature
CanCreateNewBody
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanCreateNewBody
Parameters: newBody (bool) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CanKeepParameterization¶
-
IFormBuilder.
CanKeepParameterization
¶ Returns or sets the value indicating if input surface parameterization should be preserved during deformation
-------------------------------------
Getter Method
Signature
CanKeepParameterization
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CanKeepParameterization
Parameters: canKeepParameterization (bool) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
CurveShaper¶
-
IFormBuilder.
CurveShaper
¶ Returns the iso-parameter curve shaper
-------------------------------------
Getter Method
Signature
CurveShaper
Returns: Return type: NXOpen.GeometricUtilities.CurveShapingBuilder
New in version NX7.5.0.
License requirements: None.
ExtractTolerance¶
-
IFormBuilder.
ExtractTolerance
¶ Returns or sets the tolerance used for b-surface extraction from a face
-------------------------------------
Getter Method
Signature
ExtractTolerance
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtractTolerance
Parameters: extractTolerance (float) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
FaceToDeform¶
-
IFormBuilder.
FaceToDeform
¶ Returns the face to deform.
Please refer
NXOpen.Features.FaceRecognitionBuilder
for details.-------------------------------------
Getter Method
Signature
FaceToDeform
Returns: Return type: NXOpen.Features.FaceRecognitionBuilder
New in version NX7.5.0.
License requirements: None.
InsertionMethod¶
-
IFormBuilder.
InsertionMethod
¶ Returns or sets the iso-parameter curve insertion method
-------------------------------------
Getter Method
Signature
InsertionMethod
Returns: Return type: NXOpen.Features.IFormBuilderInsertionMethodOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InsertionMethod
Parameters: insertionMethod ( NXOpen.Features.IFormBuilderInsertionMethodOptions
) –New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Number¶
-
IFormBuilder.
Number
¶ Returns or sets the number of iso-parameter curves to be inserted
-------------------------------------
Getter Method
Signature
Number
Returns: Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Number
Parameters: number (int) – New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
ParameterDirection¶
-
IFormBuilder.
ParameterDirection
¶ Returns or sets the iso-parameter direction
-------------------------------------
Getter Method
Signature
ParameterDirection
Returns: Return type: NXOpen.Features.IFormBuilderParameterDirectionOptions
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ParameterDirection
Parameters: parameterDirection ( NXOpen.Features.IFormBuilderParameterDirectionOptions
) –New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
SpecifyPoints¶
-
IFormBuilder.
SpecifyPoints
¶ Returns the specified points to define iso-parameter curve
-------------------------------------
Getter Method
Signature
SpecifyPoints
Returns: Return type: NXOpen.SelectPointList
New in version NX7.5.0.
License requirements: None.
TransitionType¶
-
IFormBuilder.
TransitionType
¶ Returns or sets the transition options for local surface deformation
-------------------------------------
Getter Method
Signature
TransitionType
Returns: Return type: NXOpen.Features.IFormBuilderTransitionTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransitionType
Parameters: transitionType ( NXOpen.Features.IFormBuilderTransitionTypes
) –New in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
UMaxContinuity¶
-
IFormBuilder.
UMaxContinuity
¶ Returns the continuity at maximum U direction
-------------------------------------
Getter Method
Signature
UMaxContinuity
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX7.5.0.
License requirements: None.
UMinContinuity¶
-
IFormBuilder.
UMinContinuity
¶ Returns the continuity at minimum U direction
-------------------------------------
Getter Method
Signature
UMinContinuity
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX7.5.0.
License requirements: None.
VMaxContinuity¶
-
IFormBuilder.
VMaxContinuity
¶ Returns the continuity at maximum U direction
-------------------------------------
Getter Method
Signature
VMaxContinuity
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX7.5.0.
License requirements: None.
VMinContinuity¶
-
IFormBuilder.
VMinContinuity
¶ Returns the continuity at minimum V direction
-------------------------------------
Getter Method
Signature
VMinContinuity
Returns: Return type: NXOpen.GeometricUtilities.Continuity
New in version NX7.5.0.
License requirements: None.
Method Detail¶
DeleteCurve¶
-
IFormBuilder.
DeleteCurve
¶ Deletes a iso-parameter curve
Signature
DeleteCurve(curve)
Parameters: curve ( NXOpen.Curve
) – Curve to be deletedNew in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
RemoveFeatureParameters¶
-
IFormBuilder.
RemoveFeatureParameters
¶ Removes parameters of a owning feature of a face to be deformed
Signature
RemoveFeatureParameters(face)
Parameters: face ( NXOpen.Face
) – Face to be used for feature parameter removalNew in version NX7.5.0.
License requirements: studio_free_form (“STUDIO FREE FORM”)
Validate¶
-
IFormBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.