DraftBodyBuilder Class¶
-
class
NXOpen.Features.
DraftBodyBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.DraftBody
builderTo create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateDraftBodyBuilder()
Default values.
Property Value DraftAngle.Value 10.0 DraftMethod Isocline ExtremeFacePointOverridesStationary False FilletRadius.Value 2.5 (millimeters part), 0.1 (inches part) MatchScope All MatchType None RepairPartingEdge None RepairRadius.Value (deprecated) 2.5 (millimeters part), 0.1 (inches part) RepairingOption (deprecated) None Type Edges UseDraftedBodyAsPartingObject False New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DraftAngle | Returns the draft angle |
DraftMethod | Returns or sets the draft method |
DrawDirection | Returns or sets the draw direction |
EdgesToMoveToDraftedFace | Returns the edges to move to drafted face |
ExtremeFacePointOverridesStationary | Returns or sets the extreme face point overrides stationary |
FacesToDraft | Returns the faces to draft |
FacesToMoveToDraftedFace | Returns the faces to move to drafted face |
FilletRadius | Returns the fillet radius |
MatchScope | Returns or sets the match scope |
MatchType | Returns or sets the match type |
MatchingOption | Returns or sets the matching option |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PartingObject | Returns the parting object |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
RepairPartingEdge | Returns or sets the repairing parting edge |
RepairRadius | Returns the repair radius |
RepairingOption | Returns or sets the repairing option |
StationaryEdgesAboveParting | Returns the stationary edges above parting |
StationaryEdgesBelowParting | Returns the stationary edges below parting |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Tolerance | Returns or sets the tolerance |
Type | Returns or sets the draft body type |
UnmatchedEdges | Returns the edges that will not be matched when matching option is AllButSelected |
UnmatchedFaces | Returns the faces that will not be matched when matching option is AllButSelected |
UseDraftedBodyAsPartingObject | Returns or sets the use drafted body as parting object |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DraftBodyBuilderMatchOption Enumeration | Describes the different match options. |
DraftBodyBuilderMatchingScope Enumeration | Describes the different match scopes. |
DraftBodyBuilderMatchingType Enumeration | Describes the different match types |
DraftBodyBuilderMethod Enumeration | Describes the Draft Body method as true draft or isocline draft. |
DraftBodyBuilderRepairOption Enumeration | Describes the different repair options. |
DraftBodyBuilderRepairingPartingEdgeOption Enumeration | Describes the different repair parting edges options. |
DraftBodyBuilderTypes Enumeration | Describes the different Draft Body types |
Property Detail¶
DraftAngle¶
-
DraftBodyBuilder.
DraftAngle
¶ Returns the draft angle
-------------------------------------
Getter Method
Signature
DraftAngle
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
License requirements: None.
DraftMethod¶
-
DraftBodyBuilder.
DraftMethod
¶ Returns or sets the draft method
-------------------------------------
Getter Method
Signature
DraftMethod
Returns: Return type: NXOpen.Features.DraftBodyBuilderMethod
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DraftMethod
Parameters: draftMethod ( NXOpen.Features.DraftBodyBuilderMethod
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
DrawDirection¶
-
DraftBodyBuilder.
DrawDirection
¶ Returns or sets the draw direction
-------------------------------------
Getter Method
Signature
DrawDirection
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrawDirection
Parameters: drawDirection ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
EdgesToMoveToDraftedFace¶
-
DraftBodyBuilder.
EdgesToMoveToDraftedFace
¶ Returns the edges to move to drafted face
-------------------------------------
Getter Method
Signature
EdgesToMoveToDraftedFace
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
ExtremeFacePointOverridesStationary¶
-
DraftBodyBuilder.
ExtremeFacePointOverridesStationary
¶ Returns or sets the extreme face point overrides stationary
-------------------------------------
Getter Method
Signature
ExtremeFacePointOverridesStationary
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtremeFacePointOverridesStationary
Parameters: extremeFacePointOverridesStationary (bool) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
FacesToDraft¶
-
DraftBodyBuilder.
FacesToDraft
¶ Returns the faces to draft
-------------------------------------
Getter Method
Signature
FacesToDraft
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
FacesToMoveToDraftedFace¶
-
DraftBodyBuilder.
FacesToMoveToDraftedFace
¶ Returns the faces to move to drafted face
-------------------------------------
Getter Method
Signature
FacesToMoveToDraftedFace
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
FilletRadius¶
-
DraftBodyBuilder.
FilletRadius
¶ Returns the fillet radius
-------------------------------------
Getter Method
Signature
FilletRadius
Returns: Return type: NXOpen.Expression
New in version NX9.0.0.
License requirements: None.
MatchScope¶
-
DraftBodyBuilder.
MatchScope
¶ Returns or sets the match scope
-------------------------------------
Getter Method
Signature
MatchScope
Returns: Return type: NXOpen.Features.DraftBodyBuilderMatchingScope
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MatchScope
Parameters: matchingScope ( NXOpen.Features.DraftBodyBuilderMatchingScope
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
MatchType¶
-
DraftBodyBuilder.
MatchType
¶ Returns or sets the match type
-------------------------------------
Getter Method
Signature
MatchType
Returns: Return type: NXOpen.Features.DraftBodyBuilderMatchingType
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MatchType
Parameters: matchType ( NXOpen.Features.DraftBodyBuilderMatchingType
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
MatchingOption¶
-
DraftBodyBuilder.
MatchingOption
¶ Returns or sets the matching option
-------------------------------------
Getter Method
Signature
MatchingOption
Returns: Return type: NXOpen.Features.DraftBodyBuilderMatchOption
New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.DraftBodyBuilder.MatchScope()
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
MatchingOption
Parameters: matchingOption ( NXOpen.Features.DraftBodyBuilderMatchOption
) –New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.DraftBodyBuilder.MatchScope()
insteadLicense requirements: solid_modeling (“SOLIDS MODELING”)
PartingObject¶
-
DraftBodyBuilder.
PartingObject
¶ Returns the parting object
-------------------------------------
Getter Method
Signature
PartingObject
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX5.0.0.
License requirements: None.
RepairPartingEdge¶
-
DraftBodyBuilder.
RepairPartingEdge
¶ Returns or sets the repairing parting edge
-------------------------------------
Getter Method
Signature
RepairPartingEdge
Returns: Return type: NXOpen.Features.DraftBodyBuilderRepairingPartingEdgeOption
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RepairPartingEdge
Parameters: repairingPartingEdges ( NXOpen.Features.DraftBodyBuilderRepairingPartingEdgeOption
) –New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RepairRadius¶
-
DraftBodyBuilder.
RepairRadius
¶ Returns the repair radius
-------------------------------------
Getter Method
Signature
RepairRadius
Returns: Return type: NXOpen.Expression
New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.DraftBodyBuilder.FilletRadius()
insteadLicense requirements: None.
RepairingOption¶
-
DraftBodyBuilder.
RepairingOption
¶ Returns or sets the repairing option
-------------------------------------
Getter Method
Signature
RepairingOption
Returns: Return type: NXOpen.Features.DraftBodyBuilderRepairOption
New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.DraftBodyBuilder.RepairPartingEdge()
insteadLicense requirements: None.
-------------------------------------
Setter Method
Signature
RepairingOption
Parameters: repairingOption ( NXOpen.Features.DraftBodyBuilderRepairOption
) –New in version NX5.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.DraftBodyBuilder.RepairPartingEdge()
insteadLicense requirements: solid_modeling (“SOLIDS MODELING”)
StationaryEdgesAboveParting¶
-
DraftBodyBuilder.
StationaryEdgesAboveParting
¶ Returns the stationary edges above parting
-------------------------------------
Getter Method
Signature
StationaryEdgesAboveParting
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
StationaryEdgesBelowParting¶
-
DraftBodyBuilder.
StationaryEdgesBelowParting
¶ Returns the stationary edges below parting
-------------------------------------
Getter Method
Signature
StationaryEdgesBelowParting
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
Tolerance¶
-
DraftBodyBuilder.
Tolerance
¶ Returns or sets the tolerance
-------------------------------------
Getter Method
Signature
Tolerance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Tolerance
Parameters: tolerance (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Type¶
-
DraftBodyBuilder.
Type
¶ Returns or sets the draft body type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.DraftBodyBuilderTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.DraftBodyBuilderTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UnmatchedEdges¶
-
DraftBodyBuilder.
UnmatchedEdges
¶ Returns the edges that will not be matched when matching option is AllButSelected
-------------------------------------
Getter Method
Signature
UnmatchedEdges
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
UnmatchedFaces¶
-
DraftBodyBuilder.
UnmatchedFaces
¶ Returns the faces that will not be matched when matching option is AllButSelected
-------------------------------------
Getter Method
Signature
UnmatchedFaces
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
UseDraftedBodyAsPartingObject¶
-
DraftBodyBuilder.
UseDraftedBodyAsPartingObject
¶ Returns or sets the use drafted body as parting object
-------------------------------------
Getter Method
Signature
UseDraftedBodyAsPartingObject
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UseDraftedBodyAsPartingObject
Parameters: useDraftedBodyAsPartingObject (bool) – New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
Validate¶
-
DraftBodyBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.