DraftBodyBuilderRepairingPartingEdgeOption Enumeration¶
NXOpen.Features.DraftBodyBuilder.RepairingPartingEdgeOption is an alias for NXOpen.Features.DraftBodyBuilderRepairingPartingEdgeOption
-
class
NXOpen.Features.
DraftBodyBuilderRepairingPartingEdgeOption
¶ Bases:
object
Describes the different repair parting edges options.
Enum Members
Enum Member Enum Member Description NotSet No repair parting edge option is specified WithFillet Repair concave miter corners with fillet WithLineAndFillet Repair concave miter corners with both fillet and line -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-