DivideCurveBuilder Class¶
-
class
NXOpen.Features.
DivideCurveBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a builder for non-associative divide curve operation.
To create a new instance of this class, use
NXOpen.Features.BaseFeatureCollection.CreateDivideCurveBuilder()
Default values.
Property Value ArcLength 1.0 CornerNumber 1 EqualArcLengthSegments 2 EqualParameterSegments 2 KnotPointNumber 1 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ArcLength | Returns or sets the arc length |
BoundingObjects | Returns the Bounding Objects list |
CornerMethod | Returns or sets the corner method |
CornerNumber | Returns or sets the corner number |
CornerPoint | Returns the corner point |
DirectionFlag | Returns or sets the input arc length direction flag |
DividingCurve | Returns the select dividing curve |
EqualArcLengthSegments | Returns or sets the equal arc length segments |
EqualParameterSegments | Returns or sets the equal parameter segments |
EqualSegmentMethod | Returns or sets the equal segment method |
KnotPoint | Returns the knot point |
KnotPointMethod | Returns or sets the knot point method |
KnotPointNumber | Returns or sets the knot point number |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the divide type |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DivideCurveBuilderCornerOption Enumeration | Represents the Divide Curve at Corner option types |
DivideCurveBuilderEqualSegmentOption Enumeration | Represents the Divide Curve equal segment method types |
DivideCurveBuilderInputArcLengthDirectionFlag Enumeration | Represents the Divide Curve Input Arc length direction flag |
DivideCurveBuilderKnotPointOption Enumeration | Represents the Divide Curve at Knot option types |
DivideCurveBuilderTypes Enumeration | Represents the Divide Curve types |
Property Detail¶
ArcLength¶
-
DivideCurveBuilder.
ArcLength
¶ Returns or sets the arc length
-------------------------------------
Getter Method
Signature
ArcLength
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcLength
Parameters: arcLength (float) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
BoundingObjects¶
-
DivideCurveBuilder.
BoundingObjects
¶ Returns the Bounding Objects list
-------------------------------------
Getter Method
Signature
BoundingObjects
Returns: Return type: NXOpen.GeometricUtilities.BoundingObjectBuilderList
New in version NX7.5.1.
License requirements: None.
CornerMethod¶
-
DivideCurveBuilder.
CornerMethod
¶ Returns or sets the corner method
-------------------------------------
Getter Method
Signature
CornerMethod
Returns: Return type: NXOpen.Features.DivideCurveBuilderCornerOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerMethod
Parameters: cornerMethod ( NXOpen.Features.DivideCurveBuilderCornerOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
CornerNumber¶
-
DivideCurveBuilder.
CornerNumber
¶ Returns or sets the corner number
-------------------------------------
Getter Method
Signature
CornerNumber
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerNumber
Parameters: cornerNumber (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
CornerPoint¶
-
DivideCurveBuilder.
CornerPoint
¶ Returns the corner point
-------------------------------------
Getter Method
Signature
CornerPoint
Returns: Return type: NXOpen.SelectPointList
New in version NX5.0.0.
License requirements: None.
DirectionFlag¶
-
DivideCurveBuilder.
DirectionFlag
¶ Returns or sets the input arc length direction flag
-------------------------------------
Getter Method
Signature
DirectionFlag
Returns: Return type: NXOpen.Features.DivideCurveBuilderInputArcLengthDirectionFlag
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DirectionFlag
Parameters: directionFlag ( NXOpen.Features.DivideCurveBuilderInputArcLengthDirectionFlag
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
DividingCurve¶
-
DivideCurveBuilder.
DividingCurve
¶ Returns the select dividing curve
-------------------------------------
Getter Method
Signature
DividingCurve
Returns: Return type: NXOpen.SelectCurve
New in version NX5.0.0.
License requirements: None.
EqualArcLengthSegments¶
-
DivideCurveBuilder.
EqualArcLengthSegments
¶ Returns or sets the equal arc length segments
-------------------------------------
Getter Method
Signature
EqualArcLengthSegments
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EqualArcLengthSegments
Parameters: equalArcLengthSegments (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
EqualParameterSegments¶
-
DivideCurveBuilder.
EqualParameterSegments
¶ Returns or sets the equal parameter segments
-------------------------------------
Getter Method
Signature
EqualParameterSegments
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EqualParameterSegments
Parameters: equalParameterSegments (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
EqualSegmentMethod¶
-
DivideCurveBuilder.
EqualSegmentMethod
¶ Returns or sets the equal segment method
-------------------------------------
Getter Method
Signature
EqualSegmentMethod
Returns: Return type: NXOpen.Features.DivideCurveBuilderEqualSegmentOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EqualSegmentMethod
Parameters: equalSegmentMethod ( NXOpen.Features.DivideCurveBuilderEqualSegmentOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
KnotPoint¶
-
DivideCurveBuilder.
KnotPoint
¶ Returns the knot point
-------------------------------------
Getter Method
Signature
KnotPoint
Returns: Return type: NXOpen.SelectPointList
New in version NX5.0.0.
License requirements: None.
KnotPointMethod¶
-
DivideCurveBuilder.
KnotPointMethod
¶ Returns or sets the knot point method
-------------------------------------
Getter Method
Signature
KnotPointMethod
Returns: Return type: NXOpen.Features.DivideCurveBuilderKnotPointOption
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KnotPointMethod
Parameters: knotPointMethod ( NXOpen.Features.DivideCurveBuilderKnotPointOption
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
KnotPointNumber¶
-
DivideCurveBuilder.
KnotPointNumber
¶ Returns or sets the knot point number
-------------------------------------
Getter Method
Signature
KnotPointNumber
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KnotPointNumber
Parameters: knotPointNumber (int) – New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Type¶
-
DivideCurveBuilder.
Type
¶ Returns or sets the divide type
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.DivideCurveBuilderTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.DivideCurveBuilderTypes
) –New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
Method Detail¶
Validate¶
-
DivideCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.