DivideCurveBuilderTypes Enumeration¶
NXOpen.Features.DivideCurveBuilder.Types is an alias for NXOpen.Features.DivideCurveBuilderTypes
-
class
NXOpen.Features.
DivideCurveBuilderTypes
¶ Bases:
object
Represents the Divide Curve types
Enum Members
Enum Member Enum Member Description EqualSegments Equal Segments ByBoundingObjects By Bounding Objects InputArcLengthSegments Input Arc Length Segments AtKnotpoints At Knotpoints AtCorners At Corners -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-