DivideCurveBuilderEqualSegmentOption Enumeration¶
NXOpen.Features.DivideCurveBuilder.EqualSegmentOption is an alias for NXOpen.Features.DivideCurveBuilderEqualSegmentOption
-
class
NXOpen.Features.
DivideCurveBuilderEqualSegmentOption
¶ Bases:
object
Represents the Divide Curve equal segment method types
Enum Members
Enum Member Enum Member Description EqualParameter Equal Parameter EqualArcLength Equal Arc length -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-