DimensionBuilder Class¶
-
class
NXOpen.Features.
DimensionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.DimensionBuilder
The sub-class should create an instance of corresponding object
Default values.
Property Value FacesToMove.CoaxialEnabled 0 FacesToMove.CoplanarAxesEnabled 0 FacesToMove.CoplanarEnabled 0 FacesToMove.EqualDiameterEnabled 0 FacesToMove.OffsetEnabled 0 FacesToMove.ParallelEnabled 0 FacesToMove.PerpendicularEnabled 0 FacesToMove.SymmetricEnabled 0 FacesToMove.TangentEnabled 0 FacesToMove.ThicknessChainEnabled 0 FacesToMove.UseFaceBrowse 1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
DimensionLocation | Returns the dimension location/placement controlled by the annotation origin block |
FaceChangeOverflowBehavior | Returns the face change overflow behavior. |
FacesToMove | Returns the faces being moved as part of the Linear Dimension command |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SaveConstraints | Returns the SaveConstraints builder which is used by ADM Dimension Features. |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Value | Returns the value of the dimension |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDimension | The drafting dimension which is used as UI tool for dimension display. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DimensionLocation¶
-
DimensionBuilder.
DimensionLocation
¶ Returns the dimension location/placement controlled by the annotation origin block
-------------------------------------
Getter Method
Signature
DimensionLocation
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX6.0.0.
License requirements: None.
FaceChangeOverflowBehavior¶
-
DimensionBuilder.
FaceChangeOverflowBehavior
¶ Returns the face change overflow behavior.
Please refer
NXOpen.GeometricUtilities.FaceChangeOverflowBehavior
for details.-------------------------------------
Getter Method
Signature
FaceChangeOverflowBehavior
Returns: Return type: NXOpen.GeometricUtilities.FaceChangeOverflowBehavior
New in version NX6.0.2.
License requirements: None.
FacesToMove¶
-
DimensionBuilder.
FacesToMove
¶ Returns the faces being moved as part of the Linear Dimension command
-------------------------------------
Getter Method
Signature
FacesToMove
Returns: Return type: NXOpen.Features.FaceRecognitionBuilder
New in version NX6.0.0.
License requirements: None.
SaveConstraints¶
-
DimensionBuilder.
SaveConstraints
¶ Returns the SaveConstraints builder which is used by ADM Dimension Features.
-------------------------------------
Getter Method
Signature
SaveConstraints
Returns: Return type: NXOpen.GeometricUtilities.SaveConstraintsBuilder
New in version NX7.0.0.
License requirements: None.
Value¶
-
DimensionBuilder.
Value
¶ Returns the value of the dimension
-------------------------------------
Getter Method
Signature
Value
Returns: Return type: NXOpen.Expression
New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetDimension¶
-
DimensionBuilder.
GetDimension
¶ The drafting dimension which is used as UI tool for dimension display.
Since this is saved with the feature, we need to create it and edit even during journalling. This command will hide all the creation and editing details of the drafting dimension. This API should be included for successful journalling
Signature
GetDimension()
Returns: Return type: NXOpen.Annotations.Dimension
New in version NX6.0.0.
License requirements: None.
Validate¶
-
DimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.