InspectionScanCurveBuilder Class¶
-
class
NXOpen.CAM.
InspectionScanCurveBuilder
¶ Bases:
NXOpen.CAM.InspectionMoveBuilder
Represents the builder for the CMM Inspection sub-operation Scan Curve.
To create a new instance of this class, use
NXOpen.CAM.InspectionMoveCollection.CreateInspectionScanCurveBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
AngleA | Returns or sets the A angle for an indexable head |
AngleB | Returns or sets the B angle for an indexable head |
ApproachDist | Returns the builder for approach distance |
ApproachDistance | Returns or sets the approach distance |
CurvatureFactor | Returns the Curvature Increase Factor for points along the Scan Curve |
Curve | Returns or sets the curve |
CurveMode | Returns or sets the curve specification mode |
DepthDistance | Returns or sets the depth distance |
DepthMethod | Returns or sets the depth method |
EndDistance | Returns or sets the End Distance of the Scan Curve |
EndDistanceBuilder | Returns the End Distance of the Scan Curve |
EndPercentage | Returns the End Percentage of the Scan Curve |
MaxSpacing | Returns the Maximum Spacing of points along the Scan Curve |
MinSpacing | Returns the Minimum Spacing of points along the Scan Curve |
MotionType | Returns or sets the motion type |
NbPointsBuilder | Returns the builder for the Number of Scan Points on the curve |
Nbpoints | Returns or sets the Number of Scan Points on the curve |
ProbeTipType | Returns or sets the preferred probe tip type |
ProbeTipTypeBuilder | Returns the Probe Tip Type Builder |
RetractDist | Returns the builder for retract distance |
RetractDistance | Returns or sets the retract distance |
Reversedirection | Returns or sets the Reverse Direction flag on the curve |
ScanSpeed | Returns the builder for scan speed |
SensorOpName | Returns or sets the inspection sensor operation name |
SensorStrategy | Returns or sets the sensor selection strategy |
SensorStrategyBuilder | Returns the Sensor Strategy Enum Builder |
StartDistance | Returns or sets the Start Distance of the Scan Curve |
StartDistanceBuilder | Returns the Start Distance of the Scan Curve |
StartEndMode | Returns or sets the start/end mode |
StartPercentage | Returns the Start Percentage of the Scan Curve |
StepSize | Returns the builder for step size |
Tag | Returns the Tag for this object. |
TipAngleMode | Returns or sets the tip angle selection mode |
TipMode | Returns or sets the probe tip selection mode |
TipNumber | Returns or sets the probe tip number |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
LockMove | Set lock to prevent move parameters from being changed programmatically. |
SetParent | Set parent |
SetProbeAngles | Set default values for probe angles based on feature type. |
SetProbeTip | Set default probe tip based on preferred tip type and probe angles. |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ApproachDist¶
-
InspectionScanCurveBuilder.
ApproachDist
¶ Returns the builder for approach distance
-------------------------------------
Getter Method
Signature
ApproachDist
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.2.
License requirements: None.
CurvatureFactor¶
-
InspectionScanCurveBuilder.
CurvatureFactor
¶ Returns the Curvature Increase Factor for points along the Scan Curve
-------------------------------------
Getter Method
Signature
CurvatureFactor
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.3.
License requirements: None.
Curve¶
-
InspectionScanCurveBuilder.
Curve
¶ Returns or sets the curve
-------------------------------------
Getter Method
Signature
Curve
Returns: Return type: NXOpen.NXObject
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Curve
Parameters: curve ( NXOpen.NXObject
) –New in version NX7.0.0.
License requirements: None.
CurveMode¶
-
InspectionScanCurveBuilder.
CurveMode
¶ Returns or sets the curve specification mode
-------------------------------------
Getter Method
Signature
CurveMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderScanCurveModeTypes
New in version NX7.5.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurveMode
Parameters: mode ( NXOpen.CAM.InspectionMethodBuilderScanCurveModeTypes
) –New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthDistance¶
-
InspectionScanCurveBuilder.
DepthDistance
¶ Returns or sets the depth distance
-------------------------------------
Getter Method
Signature
DepthDistance
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthDistance
Parameters: distance (float) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
DepthMethod¶
-
InspectionScanCurveBuilder.
DepthMethod
¶ Returns or sets the depth method
-------------------------------------
Getter Method
Signature
DepthMethod
Returns: Return type: NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthMethod
Parameters: method ( NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
) –New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndDistance¶
-
InspectionScanCurveBuilder.
EndDistance
¶ Returns or sets the End Distance of the Scan Curve
-------------------------------------
Getter Method
Signature
EndDistance
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndDistance
Parameters: distance (float) – New in version NX7.0.0.
License requirements: None.
EndDistanceBuilder¶
-
InspectionScanCurveBuilder.
EndDistanceBuilder
¶ Returns the End Distance of the Scan Curve
-------------------------------------
Getter Method
Signature
EndDistanceBuilder
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
EndPercentage¶
-
InspectionScanCurveBuilder.
EndPercentage
¶ Returns the End Percentage of the Scan Curve
-------------------------------------
Getter Method
Signature
EndPercentage
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
MaxSpacing¶
-
InspectionScanCurveBuilder.
MaxSpacing
¶ Returns the Maximum Spacing of points along the Scan Curve
-------------------------------------
Getter Method
Signature
MaxSpacing
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.3.
License requirements: None.
MinSpacing¶
-
InspectionScanCurveBuilder.
MinSpacing
¶ Returns the Minimum Spacing of points along the Scan Curve
-------------------------------------
Getter Method
Signature
MinSpacing
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.3.
License requirements: None.
NbPointsBuilder¶
-
InspectionScanCurveBuilder.
NbPointsBuilder
¶ Returns the builder for the Number of Scan Points on the curve
-------------------------------------
Getter Method
Signature
NbPointsBuilder
Returns: Return type: NXOpen.CAM.InheritableIntBuilder
New in version NX8.5.0.
License requirements: None.
Nbpoints¶
-
InspectionScanCurveBuilder.
Nbpoints
¶ Returns or sets the Number of Scan Points on the curve
-------------------------------------
Getter Method
Signature
Nbpoints
Returns: Return type: int New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Nbpoints
Parameters: nbpoints (int) – New in version NX7.0.0.
License requirements: None.
RetractDist¶
-
InspectionScanCurveBuilder.
RetractDist
¶ Returns the builder for retract distance
-------------------------------------
Getter Method
Signature
RetractDist
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.2.
License requirements: None.
Reversedirection¶
-
InspectionScanCurveBuilder.
Reversedirection
¶ Returns or sets the Reverse Direction flag on the curve
-------------------------------------
Getter Method
Signature
Reversedirection
Returns: Return type: bool New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Reversedirection
Parameters: reversedir (bool) – New in version NX7.0.0.
License requirements: None.
ScanSpeed¶
-
InspectionScanCurveBuilder.
ScanSpeed
¶ Returns the builder for scan speed
-------------------------------------
Getter Method
Signature
ScanSpeed
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.0.
License requirements: None.
StartDistance¶
-
InspectionScanCurveBuilder.
StartDistance
¶ Returns or sets the Start Distance of the Scan Curve
-------------------------------------
Getter Method
Signature
StartDistance
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartDistance
Parameters: distance (float) – New in version NX7.0.0.
License requirements: None.
StartDistanceBuilder¶
-
InspectionScanCurveBuilder.
StartDistanceBuilder
¶ Returns the Start Distance of the Scan Curve
-------------------------------------
Getter Method
Signature
StartDistanceBuilder
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
StartEndMode¶
-
InspectionScanCurveBuilder.
StartEndMode
¶ Returns or sets the start/end mode
-------------------------------------
Getter Method
Signature
StartEndMode
Returns: Return type: NXOpen.CAM.InspectionMethodBuilderUVModeTypes
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartEndMode
Parameters: startEndMode ( NXOpen.CAM.InspectionMethodBuilderUVModeTypes
) –New in version NX8.5.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartPercentage¶
-
InspectionScanCurveBuilder.
StartPercentage
¶ Returns the Start Percentage of the Scan Curve
-------------------------------------
Getter Method
Signature
StartPercentage
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX8.5.0.
License requirements: None.
StepSize¶
-
InspectionScanCurveBuilder.
StepSize
¶ Returns the builder for step size
-------------------------------------
Getter Method
Signature
StepSize
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
InspectionScanCurveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.