InspectionMoveBuilderDepthMethodTypes Enumeration¶
NXOpen.CAM.InspectionMoveBuilder.DepthMethodTypes is an alias for NXOpen.CAM.InspectionMoveBuilderDepthMethodTypes
-
class
NXOpen.CAM.
InspectionMoveBuilderDepthMethodTypes
¶ Bases:
object
the depth method
Enum Members
Enum Member Enum Member Description Auto Auto specify Distance Distance only FromFeatureNominal Distance from feature nominal FromFeatureActual Distance from feature actual FromDatum Distance from datum -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-