CenterlineDrillTurningBuilder Class¶
-
class
NXOpen.CAM.
CenterlineDrillTurningBuilder
¶ Bases:
NXOpen.CAM.TurningOperationBuilder
Represents a CenterlineDrillTurningBuilder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateCenterlineDrillTurningBuilder()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
AdditionalCommands | Returns or sets the Additional Commands |
BreakThrough | Returns or sets the break through toggle IMPORTANT: Parameter is obsolete from NX9 on and must not be used longer. |
BreakThroughDistance | Returns the break through distance IMPORTANT: Parameter is obsolete from NX9 on and must not be used longer. |
CenterlineCycle | Returns or sets the centerline cycle |
ChannelName | Returns or sets the channel’s name |
ChipRemovalIncrementType | Returns or sets the chip removal increment type |
ClearanceDistance | Returns the clearance distance |
ConstantIncrement | Returns the constant increment |
CrossHoleAngle | Returns the cross hole angle |
CrossHoleCircle | Returns or sets the cross hole circle |
CrossHoleDiameter | Returns the cross hole diameter |
CrossHoleDistance | Returns the cross hole distance |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
DepthDistance | Returns the depth distance |
DepthEndPoint | Returns or sets the depth end point |
DepthOffset | Returns the depth offset value |
DepthOption | Returns or sets the depth option |
DepthReference | Returns or sets the depth reference |
Description | Returns or sets the description |
DrillStep | Returns the drill step |
DrillStepModifier1 | Returns the drill step modifier1 |
DrillStepModifier2 | Returns the drill step modifier2 |
DrillingLocation | Returns or sets the drilling location |
DwellType | Returns or sets the dwell type |
DwellValue | Returns the dwell value |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
EngageDistance | Returns the engage distance |
EntranceDiameter | Returns the entrance diameter |
FeedsBuilder | Returns the feeds and speeds builder |
FinalRetractDistance | Returns the retract distance for simulated cycles |
FinalRetractType | Returns or sets the retract type for simulated cycles |
FlipToolAroundHolder | Returns or sets the Flip Tool Around Holder toggle |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MachineCycleSubroutineName | Returns or sets the machine cycle subroutine name |
MotionOutput | Returns or sets the motion output |
MotionOutputBuilder | Returns the motion output builder |
NonCuttingBuilder | Returns the non-cutting builder |
Notes | Returns the notes builder |
OffCenterDistance | Returns the off center distance |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
OutputOption | Returns or sets the output option |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
ReorientToolHolder | Returns or sets the Reorient Tool Holder toggle. |
ReorientToolHolderMode | Returns or sets the Reorient Tool Holder Mode |
RepositionDistance | Returns the reposition distance |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
ReverseDirection | Returns or sets the reverse direction value |
RotateTrackingPoint | Returns or sets the Rotate Tracking Point toggle |
SafeClearance | Returns the safe clearance builder |
SafeOrDepartureDistance | Returns the safe or departure distance |
SelectToolFlag | Returns or sets the user selected tool |
SpindleStop | Returns or sets the spindle stop |
StartOfPath | Returns the start event builder |
StartPosition | Returns or sets the start position |
StartPositionPoint | Returns or sets the start position point |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolHolderAngle | Returns the Tool Holder Angle |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
TrackingPointStatus | Returns or sets the tracking point status |
UpdateIpw | Returns or sets the update IPW mode |
UseMachineCycle | Returns or sets the Use Machine Cycle toggle |
VariableIncrementList | Returns the variable increment list |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetCycleTrackingPoint | Returns the cycle tracking point |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetCycleTrackingPoint | Sets the cycle tracking point |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CenterlineDrillTurningBuilderCycleTypes Enumeration | the centerline cycle types |
CenterlineDrillTurningBuilderDepthReferenceTypes Enumeration | the depth reference option types |
CenterlineDrillTurningBuilderDepthTypes Enumeration | the depth option types |
CenterlineDrillTurningBuilderDrillingLocationTypes Enumeration | the drilling location |
CenterlineDrillTurningBuilderDwellTypes Enumeration | the dwell modes |
CenterlineDrillTurningBuilderFinalRetractTypes Enumeration | the retract types for simulated cycles |
CenterlineDrillTurningBuilderOutputOptionTypes Enumeration | the output option |
CenterlineDrillTurningBuilderRemovalIncrementTypes Enumeration | the removal increment types |
CenterlineDrillTurningBuilderSpindleStopTypes Enumeration | the spindle stop types |
CenterlineDrillTurningBuilderStartPositionTypes Enumeration | the start position |
Property Detail¶
BreakThrough¶
-
CenterlineDrillTurningBuilder.
BreakThrough
¶ Returns or sets the break through toggle IMPORTANT: Parameter is obsolete from NX9 on and must not be used longer.
-------------------------------------
Getter Method
Signature
BreakThrough
Returns: the break through flag value Return type: bool New in version NX6.0.0.
Deprecated since version NX9.0.0: Use ‘depth reference’ instead.
License requirements: None.
-------------------------------------
Setter Method
Signature
BreakThrough
Parameters: breakThroughFlag (bool) – the break through flag value New in version NX6.0.0.
Deprecated since version NX9.0.0: Use ‘depth reference’ instead.
License requirements: cam_base (“CAM BASE”)
BreakThroughDistance¶
-
CenterlineDrillTurningBuilder.
BreakThroughDistance
¶ Returns the break through distance IMPORTANT: Parameter is obsolete from NX9 on and must not be used longer.
-------------------------------------
Getter Method
Signature
BreakThroughDistance
Returns: the break through distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use ‘depth offset’ instead.
License requirements: None.
CenterlineCycle¶
-
CenterlineDrillTurningBuilder.
CenterlineCycle
¶ Returns or sets the centerline cycle
-------------------------------------
Getter Method
Signature
CenterlineCycle
Returns: the cycle Return type: NXOpen.CAM.CenterlineDrillTurningBuilderCycleTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterlineCycle
Parameters: cycleMode ( NXOpen.CAM.CenterlineDrillTurningBuilderCycleTypes
) – the cycleNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ChipRemovalIncrementType¶
-
CenterlineDrillTurningBuilder.
ChipRemovalIncrementType
¶ Returns or sets the chip removal increment type
-------------------------------------
Getter Method
Signature
ChipRemovalIncrementType
Returns: the chip removal increment type Return type: NXOpen.CAM.CenterlineDrillTurningBuilderRemovalIncrementTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChipRemovalIncrementType
Parameters: incrementType ( NXOpen.CAM.CenterlineDrillTurningBuilderRemovalIncrementTypes
) – the removal increment typeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ClearanceDistance¶
-
CenterlineDrillTurningBuilder.
ClearanceDistance
¶ Returns the clearance distance
-------------------------------------
Getter Method
Signature
ClearanceDistance
Returns: the clearance distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
ConstantIncrement¶
-
CenterlineDrillTurningBuilder.
ConstantIncrement
¶ Returns the constant increment
-------------------------------------
Getter Method
Signature
ConstantIncrement
Returns: the constant increment Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
CrossHoleAngle¶
-
CenterlineDrillTurningBuilder.
CrossHoleAngle
¶ Returns the cross hole angle
-------------------------------------
Getter Method
Signature
CrossHoleAngle
Returns: the cross hole angle builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
CrossHoleCircle¶
-
CenterlineDrillTurningBuilder.
CrossHoleCircle
¶ Returns or sets the cross hole circle
-------------------------------------
Getter Method
Signature
CrossHoleCircle
Returns: the cross hole circle Return type: NXOpen.NXObject
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CrossHoleCircle
Parameters: crossHoleCircle ( NXOpen.NXObject
) – the cross hole circleNew in version NX7.0.0.
License requirements: cam_base (“CAM BASE”)
CrossHoleDiameter¶
-
CenterlineDrillTurningBuilder.
CrossHoleDiameter
¶ Returns the cross hole diameter
-------------------------------------
Getter Method
Signature
CrossHoleDiameter
Returns: the cross hole diameter Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
CrossHoleDistance¶
-
CenterlineDrillTurningBuilder.
CrossHoleDistance
¶ Returns the cross hole distance
-------------------------------------
Getter Method
Signature
CrossHoleDistance
Returns: the cross hole distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
DepthDistance¶
-
CenterlineDrillTurningBuilder.
DepthDistance
¶ Returns the depth distance
-------------------------------------
Getter Method
Signature
DepthDistance
Returns: the off center distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
DepthEndPoint¶
-
CenterlineDrillTurningBuilder.
DepthEndPoint
¶ Returns or sets the depth end point
-------------------------------------
Getter Method
Signature
DepthEndPoint
Returns: the depth end point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthEndPoint
Parameters: endPoint ( NXOpen.Point
) – the depth end pointNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
DepthOffset¶
-
CenterlineDrillTurningBuilder.
DepthOffset
¶ Returns the depth offset value
-------------------------------------
Getter Method
Signature
DepthOffset
Returns: the depth offset builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
DepthOption¶
-
CenterlineDrillTurningBuilder.
DepthOption
¶ Returns or sets the depth option
-------------------------------------
Getter Method
Signature
DepthOption
Returns: the depth option Return type: NXOpen.CAM.CenterlineDrillTurningBuilderDepthTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthOption
Parameters: depthOption ( NXOpen.CAM.CenterlineDrillTurningBuilderDepthTypes
) – the depth optionNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
DepthReference¶
-
CenterlineDrillTurningBuilder.
DepthReference
¶ Returns or sets the depth reference
-------------------------------------
Getter Method
Signature
DepthReference
Returns: the depth reference Return type: NXOpen.CAM.CenterlineDrillTurningBuilderDepthReferenceTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DepthReference
Parameters: depthReference ( NXOpen.CAM.CenterlineDrillTurningBuilderDepthReferenceTypes
) – the depth referenceNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
DrillStep¶
-
CenterlineDrillTurningBuilder.
DrillStep
¶ Returns the drill step
-------------------------------------
Getter Method
Signature
DrillStep
Returns: the step Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
DrillStepModifier1¶
-
CenterlineDrillTurningBuilder.
DrillStepModifier1
¶ Returns the drill step modifier1
-------------------------------------
Getter Method
Signature
DrillStepModifier1
Returns: the step modifier1 Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
DrillStepModifier2¶
-
CenterlineDrillTurningBuilder.
DrillStepModifier2
¶ Returns the drill step modifier2
-------------------------------------
Getter Method
Signature
DrillStepModifier2
Returns: the step modifier2 Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
DrillingLocation¶
-
CenterlineDrillTurningBuilder.
DrillingLocation
¶ Returns or sets the drilling location
-------------------------------------
Getter Method
Signature
DrillingLocation
Returns: the drilling location Return type: NXOpen.CAM.CenterlineDrillTurningBuilderDrillingLocationTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrillingLocation
Parameters: drillingLocationMode ( NXOpen.CAM.CenterlineDrillTurningBuilderDrillingLocationTypes
) – the drilling locationNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
DwellType¶
-
CenterlineDrillTurningBuilder.
DwellType
¶ Returns or sets the dwell type
-------------------------------------
Getter Method
Signature
DwellType
Returns: the dwell type Return type: NXOpen.CAM.CenterlineDrillTurningBuilderDwellTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DwellType
Parameters: dwellMode ( NXOpen.CAM.CenterlineDrillTurningBuilderDwellTypes
) – the dwell typeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
DwellValue¶
-
CenterlineDrillTurningBuilder.
DwellValue
¶ Returns the dwell value
-------------------------------------
Getter Method
Signature
DwellValue
Returns: the dwell value Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
EngageDistance¶
-
CenterlineDrillTurningBuilder.
EngageDistance
¶ Returns the engage distance
-------------------------------------
Getter Method
Signature
EngageDistance
Returns: the engage distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
EntranceDiameter¶
-
CenterlineDrillTurningBuilder.
EntranceDiameter
¶ Returns the entrance diameter
-------------------------------------
Getter Method
Signature
EntranceDiameter
Returns: the entrance diameter builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
FinalRetractDistance¶
-
CenterlineDrillTurningBuilder.
FinalRetractDistance
¶ Returns the retract distance for simulated cycles
-------------------------------------
Getter Method
Signature
FinalRetractDistance
Returns: the retract distance for simulated cycles Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
FinalRetractType¶
-
CenterlineDrillTurningBuilder.
FinalRetractType
¶ Returns or sets the retract type for simulated cycles
-------------------------------------
Getter Method
Signature
FinalRetractType
Returns: the final retract type for simulated cycles Return type: NXOpen.CAM.CenterlineDrillTurningBuilderFinalRetractTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FinalRetractType
Parameters: finalRetractType ( NXOpen.CAM.CenterlineDrillTurningBuilderFinalRetractTypes
) – the retract type for simulated cyclesNew in version NX7.5.0.
License requirements: None.
NonCuttingBuilder¶
-
CenterlineDrillTurningBuilder.
NonCuttingBuilder
¶ Returns the non-cutting builder
-------------------------------------
Getter Method
Signature
NonCuttingBuilder
Returns: the non-cutting builder Return type: NXOpen.CAM.NcmTurningBuilder
New in version NX6.0.0.
License requirements: None.
OffCenterDistance¶
-
CenterlineDrillTurningBuilder.
OffCenterDistance
¶ Returns the off center distance
-------------------------------------
Getter Method
Signature
OffCenterDistance
Returns: the off center distance builder Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
OutputOption¶
-
CenterlineDrillTurningBuilder.
OutputOption
¶ Returns or sets the output option
-------------------------------------
Getter Method
Signature
OutputOption
Returns: the output option mode Return type: NXOpen.CAM.CenterlineDrillTurningBuilderOutputOptionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OutputOption
Parameters: outputOptionMode ( NXOpen.CAM.CenterlineDrillTurningBuilderOutputOptionTypes
) – the output option modeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
RepositionDistance¶
-
CenterlineDrillTurningBuilder.
RepositionDistance
¶ Returns the reposition distance
-------------------------------------
Getter Method
Signature
RepositionDistance
Returns: the reposition distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX7.5.0.
License requirements: None.
ReverseDirection¶
-
CenterlineDrillTurningBuilder.
ReverseDirection
¶ Returns or sets the reverse direction value
-------------------------------------
Getter Method
Signature
ReverseDirection
Returns: the reverse direction value Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseDirection
Parameters: isReverseDirection (bool) – the reverse direction value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SafeOrDepartureDistance¶
-
CenterlineDrillTurningBuilder.
SafeOrDepartureDistance
¶ Returns the safe or departure distance
-------------------------------------
Getter Method
Signature
SafeOrDepartureDistance
Returns: the safe or departure distance Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX6.0.0.
License requirements: None.
SpindleStop¶
-
CenterlineDrillTurningBuilder.
SpindleStop
¶ Returns or sets the spindle stop
-------------------------------------
Getter Method
Signature
SpindleStop
Returns: the spindle stop Return type: NXOpen.CAM.CenterlineDrillTurningBuilderSpindleStopTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SpindleStop
Parameters: spindleStop ( NXOpen.CAM.CenterlineDrillTurningBuilderSpindleStopTypes
) – the spindle stopNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
StartPosition¶
-
CenterlineDrillTurningBuilder.
StartPosition
¶ Returns or sets the start position
-------------------------------------
Getter Method
Signature
StartPosition
Returns: the start position Return type: NXOpen.CAM.CenterlineDrillTurningBuilderStartPositionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPosition
Parameters: startPositionMode ( NXOpen.CAM.CenterlineDrillTurningBuilderStartPositionTypes
) – the start position modeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
StartPositionPoint¶
-
CenterlineDrillTurningBuilder.
StartPositionPoint
¶ Returns or sets the start position point
-------------------------------------
Getter Method
Signature
StartPositionPoint
Returns: the start position point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPositionPoint
Parameters: startPositionSpecifyPoint ( NXOpen.Point
) – the start position pointNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
VariableIncrementList¶
-
CenterlineDrillTurningBuilder.
VariableIncrementList
¶ Returns the variable increment list
-------------------------------------
Getter Method
Signature
VariableIncrementList
Returns: the variable increment list Return type: NXOpen.CAM.CenterlineDrillVariableIncrementBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
GetCycleTrackingPoint¶
-
CenterlineDrillTurningBuilder.
GetCycleTrackingPoint
¶ Returns the cycle tracking point
Signature
GetCycleTrackingPoint()
Returns: Return type: str New in version NX10.0.2.
License requirements: None.
SetCycleTrackingPoint¶
-
CenterlineDrillTurningBuilder.
SetCycleTrackingPoint
¶ Sets the cycle tracking point
Signature
SetCycleTrackingPoint(name)
Parameters: name (str) – New in version NX10.0.2.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
CenterlineDrillTurningBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.