CenterlineDrillTurningBuilderCycleTypes Enumeration¶
NXOpen.CAM.CenterlineDrillTurningBuilder.CycleTypes is an alias for NXOpen.CAM.CenterlineDrillTurningBuilderCycleTypes
-
class
NXOpen.CAM.
CenterlineDrillTurningBuilderCycleTypes
¶ Bases:
object
the centerline cycle types
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description Drill Cycle: Drill DrillDeep Cycle: Drill, Deep DrillBreakChip Cycle: Drill, Break Chip Tap Cycle: Tap TapFloat Cycle: Tap, Float Bore Cycle: Bore -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-