CenterlineDrillVariableIncrementBuilder Class¶
-
class
NXOpen.CAM.
CenterlineDrillVariableIncrementBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a Turn Avoidance Path Points Builder
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
DeleteVariableIncrementListData | Delete an existing variable increment |
GetVariableIncrementListData | Get the values of variable increment |
ModifyVariableIncrementListData | Modify an existing variable increment value, name maybe changed if not unique |
SetVariableIncrementListData | Create a new variable increment at last of list, name maybe changed if not unique |
Method Detail¶
DeleteVariableIncrementListData¶
-
CenterlineDrillVariableIncrementBuilder.
DeleteVariableIncrementListData
¶ Delete an existing variable increment
Signature
DeleteVariableIncrementListData(index)
Parameters: index (int) – the index of deleted variable increment list New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
GetVariableIncrementListData¶
-
CenterlineDrillVariableIncrementBuilder.
GetVariableIncrementListData
¶ Get the values of variable increment
Signature
GetVariableIncrementListData(index)
Parameters: index (int) – the index which will be get Returns: a tuple Return type: A tuple consisting of (numberOfCuts, increment) numberOfCuts is a int. the number of cuts increment is a float. the increment value New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
ModifyVariableIncrementListData¶
-
CenterlineDrillVariableIncrementBuilder.
ModifyVariableIncrementListData
¶ Modify an existing variable increment value, name maybe changed if not unique
Signature
ModifyVariableIncrementListData(index, numberOfCuts, increment)
Parameters: - index (int) – the index of modified variable increment
- numberOfCuts (int) – the number of cuts
- increment (float) – the increment value
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
SetVariableIncrementListData¶
-
CenterlineDrillVariableIncrementBuilder.
SetVariableIncrementListData
¶ Create a new variable increment at last of list, name maybe changed if not unique
Signature
SetVariableIncrementListData(numberOfCuts, increment)
Parameters: - numberOfCuts (int) – the number of cuts
- increment (float) – the increment value
New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)