public interface ProxyPort extends Port, IAxisPort
ProxyPort
is a port that represents a connector in
another design zone, but not present in this design zone. ProxyPort
can be assigned to a connector using the ConnectorDevice
class method ConnectorDevice.proxyAssignConnector(nxopen.routing.Port)
Routing.ProxyPortCollection#createProxyPort
Port.ConnectedPortsData, Port.CreateRotationVector, Port.FlowDirectionType, Port.PortType
SmartObject.UpdateOption, SmartObject.VisibilityOption
DisplayableObject.ObjectFont, DisplayableObject.ObjectWidth
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
double |
backwardExtension()
|
Expression |
backwardExtensionObject()
Returns the backward extension object for a port, i.e. an expression representing the minimum
length that a segment must remain straight before entering a
Port
License requirements: routing_base ("Routing Basic") Created in NX8.0.0 |
void |
setBackwardExtension(double backwardExtension)
|
void |
setBackwardExtensionObject(Expression backwardExtension)
Sets the backward extension object for a port, i.e. an expression representing the minimum
length that a segment must remain straight before entering a
Port
License requirements: routing_base ("Routing Basic") Created in NX8.0.0 |
allowMultipleConnections, askFeature, clockIncrementObject, connect, disconnect, findPortIntegerCharacteristic, findPortRealCharacteristic, findPortStringCharacteristic, getAlignmentVector, getClockIncrement, getComponent, getConnectedPorts, getControlPoint, getCutbackLength, getEngagement, getFlowDirection, getForwardExtension, getPortConnection, getPortType, getReferenceCharacteristic, getRotationObject, getRotationVector, getSegment, getStockOfPort, isEngagementLocked, isRotationLocked, lockEngagement, lockRotation, reorderFeature, setAllowMultipleConnections, setClockIncrement, setClockIncrementObject, setFlowDirection, setReferenceCharacteristic, unlockEngagement, unlockRotation
evaluate, removeParameters, replaceParameters, setVisibility, update, visibility
blank, color, highlight, isBlanked, layer, lineFont, lineWidth, nameLocation, redisplayObject, removeViewDependency, setColor, setLayer, setLineFont, setLineWidth, setNameLocation, unblank, unhighlight
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
axis, cutbackLengthObject, engagementObject, forwardExtensionObject, setAlignVector, setAxis, setCutbackLength, setCutbackLengthObject, setEngagement, setEngagementObject, setForwardExtension, setForwardExtensionObject, setRotationObject, setRotationVector
point, position, setPoint, setPosition
deleteCharacterstics, getCharacteristics, getDestinationCharacteristics, getIntegerCharacteristic, getRealCharacteristic, getStringCharacteristic, setCharacteristic, setCharacteristic, setCharacteristic, setCharacteristic2, setCharacteristic2, setCharacteristic2, setCharacteristics, setCharacteristics2
double backwardExtension() throws NXException, RemoteException
ProxyPort
,
i.e. the minimum length that a segment must remain straight
before entering a ProxyPort
NXException
RemoteException
void setBackwardExtension(double backwardExtension) throws NXException, RemoteException
ProxyPort
,
i.e. the minimum length that a segment must remain straight
before entering a ProxyPort
backwardExtension
- back extension lengthNXException
RemoteException
Expression backwardExtensionObject() throws NXException, RemoteException
Port
NXException
RemoteException
void setBackwardExtensionObject(Expression backwardExtension) throws NXException, RemoteException
Port
backwardExtension
- Backward Extension ExpressionNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.