public static class Port.CreateRotationVector extends Enum
FittingPortCollection.createFromCsys(nxopen.CartesianCoordinateSystem, nxopen.routing.Port.CreateRotationVector)
and
Routing.FixturePortCollection#createFromCsys
to determine if
the rotation vector on the port should be created.Modifier and Type | Field and Description |
---|---|
static int |
_NO
Do not create the rotation vector on the port created from a coordinate system.
|
static int |
_YES
Create the rotation vector on the port created from a coordinate system.
|
static Port.CreateRotationVector |
NO
Do not create the rotation vector on the port created from a coordinate system.
|
static Port.CreateRotationVector |
YES
Create the rotation vector on the port created from a coordinate system.
|
Modifier and Type | Method and Description |
---|---|
static Port.CreateRotationVector |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Port.CreateRotationVector |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Port.CreateRotationVector[] |
values()
Returns an array that contains the values for this enum.
|
public static final Port.CreateRotationVector NO
public static final Port.CreateRotationVector YES
public static final int _NO
public static final int _YES
public static Port.CreateRotationVector valueOf(int value)
public static Port.CreateRotationVector valueOf(String name)
public static Port.CreateRotationVector[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.