public interface IRoutePosition extends ICharacteristic
Modifier and Type | Method and Description |
---|---|
Point |
point()
Returns the
Point that specifies the location of the
IRoutePosition object. |
Point3d |
position()
Returns the current location of the object in ABS coordinates.
|
void |
setPoint(Point point)
Sets the
Point that specifies the location of the
IRoutePosition object. |
void |
setPosition(Point3d position)
Sets the current location of the object in ABS coordinates.
|
deleteCharacterstics, getCharacteristics, getDestinationCharacteristics, getIntegerCharacteristic, getRealCharacteristic, getStringCharacteristic, setCharacteristic, setCharacteristic, setCharacteristic, setCharacteristic2, setCharacteristic2, setCharacteristic2, setCharacteristics, setCharacteristics2
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
Point3d position() throws NXException, RemoteException
NXException
RemoteException
void setPosition(Point3d position) throws NXException, RemoteException
position
- New location of object in ABS coordinatesNXException
RemoteException
Point point() throws NXException, RemoteException
Point
that specifies the location of the
IRoutePosition
object. A NULL object indicates that this
object is not associated to any point.
NXException
RemoteException
void setPoint(Point point) throws NXException, RemoteException
Point
that specifies the location of the
IRoutePosition
object. A NULL object indicates that this
object is not associated to any point.
point
- New location of object in ABS coordinatesNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.