public interface FixturePort extends Port, IAxisPort
FixturePort
objects are objects that
segments are routed through when creating a routing path. Routing.FixturePortCollection#createFixturePort
Port.ConnectedPortsData, Port.CreateRotationVector, Port.FlowDirectionType, Port.PortType
SmartObject.UpdateOption, SmartObject.VisibilityOption
DisplayableObject.ObjectFont, DisplayableObject.ObjectWidth
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
double |
backwardExtension()
Returns the backward extension of
FixturePort ,
i.e. the minimum length that a segment must remain straight
before entering a FixturePort
License requirements: routing_base ("Routing Basic") Created in NX4.0.0 |
Expression |
backwardExtensionObject()
Returns the backward extension object for a port, i.e. an expression representing the minimum
length that a segment must remain straight before entering a
Port
License requirements: routing_base ("Routing Basic") Created in NX4.0.0 |
void |
setBackwardExtension(double backwardExtension)
Sets the backward extension of
FixturePort ,
i.e. the minimum length that a segment must remain straight
before entering a FixturePort
License requirements: routing_base ("Routing Basic") Created in NX4.0.0 |
void |
setBackwardExtensionObject(Expression backwardExtension)
Sets the backward extension object for a port, i.e. an expression representing the minimum
length that a segment must remain straight before entering a
Port
License requirements: routing_base ("Routing Basic") Created in NX4.0.0 |
allowMultipleConnections, askFeature, clockIncrementObject, connect, disconnect, findPortIntegerCharacteristic, findPortRealCharacteristic, findPortStringCharacteristic, getAlignmentVector, getClockIncrement, getComponent, getConnectedPorts, getControlPoint, getCutbackLength, getEngagement, getFlowDirection, getForwardExtension, getPortConnection, getPortType, getReferenceCharacteristic, getRotationObject, getRotationVector, getSegment, getStockOfPort, isEngagementLocked, isRotationLocked, lockEngagement, lockRotation, reorderFeature, setAllowMultipleConnections, setClockIncrement, setClockIncrementObject, setFlowDirection, setReferenceCharacteristic, unlockEngagement, unlockRotation
evaluate, removeParameters, replaceParameters, setVisibility, update, visibility
blank, color, highlight, isBlanked, layer, lineFont, lineWidth, nameLocation, redisplayObject, removeViewDependency, setColor, setLayer, setLineFont, setLineWidth, setNameLocation, unblank, unhighlight
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
findObject, isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
axis, cutbackLengthObject, engagementObject, forwardExtensionObject, setAlignVector, setAxis, setCutbackLength, setCutbackLengthObject, setEngagement, setEngagementObject, setForwardExtension, setForwardExtensionObject, setRotationObject, setRotationVector
point, position, setPoint, setPosition
deleteCharacterstics, getCharacteristics, getDestinationCharacteristics, getIntegerCharacteristic, getRealCharacteristic, getStringCharacteristic, setCharacteristic, setCharacteristic, setCharacteristic, setCharacteristic2, setCharacteristic2, setCharacteristic2, setCharacteristics, setCharacteristics2
double backwardExtension() throws NXException, RemoteException
FixturePort
,
i.e. the minimum length that a segment must remain straight
before entering a FixturePort
NXException
RemoteException
void setBackwardExtension(double backwardExtension) throws NXException, RemoteException
FixturePort
,
i.e. the minimum length that a segment must remain straight
before entering a FixturePort
backwardExtension
- back extension lengthNXException
RemoteException
Expression backwardExtensionObject() throws NXException, RemoteException
Port
NXException
RemoteException
void setBackwardExtensionObject(Expression backwardExtension) throws NXException, RemoteException
Port
backwardExtension
- Backward Extension ExpressionNXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.