Interface | Description |
---|---|
ColumnFeature |
Represents a column feature feature
To create or edit an instance of this class, use ColumnFeatureBuilder Created in NX9.0.0 |
ColumnFeatureBuilder |
Represents a
LineDesigner.ColumnFeature Features.FeatureBuilder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createColumnFeatureBuilder Default values. |
ColumnGridEquipmentBuilder |
Represents a LineDesigner.ColumnGridEquipment builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createColumnGridEquipmentBuilder Default values. |
ConnectionCreatorBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createConnectionCreatorBuilder Default values. |
ConveyorStationFeature |
Represents a conveyor station feature feature
To create or edit an instance of this class, use ConveyorStationFeatureBuilder Created in NX9.0.0 |
ConveyorStationFeatureBuilder |
Represents a
LineDesigner.ConveyorStationFeature builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createConveyorStationFeatureBuilder Default values. |
CoverFeature |
Represents a cover feature
To create or edit an instance of this class, use CoverFeatureBuilder Created in NX9.0.0 |
CoverFeatureBuilder |
Represents a
LineDesigner.CoverFeature builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createCoverFeatureBuilder Default values. |
CreateFactoryElement |
Represents a create factory element
To create or edit an instance of this class, use CreateFactoryElementBuilder Created in NX9.0.0 |
CreateFactoryElementBuilder |
Represents a
LineDesigner.CreateFactoryElement builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createCreateFactoryElementBuilder Default values. |
CreateFence |
Represents a create fence
To create or edit an instance of this class, use CreateFenceBuilder Created in NX9.0.0 |
CreateFenceBuilder |
Represents a
LineDesigner.CreateFence builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createCreateFenceBuilder Created in NX9.0.0 |
CreateSystem |
Represents a create system
To create or edit an instance of this class, use CreateSystemBuilder Created in NX9.0.0 |
CreateSystemBuilder |
Represents a
LineDesigner.CreateSystem builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createCreateSystemBuilder Created in NX9.0.0 |
DBColumnGridNode |
Represents DB column grid node
To create a new instance of this class, use DBNodeManager.createDBColumnGridNode(nxopen.Part) Created in NX9.0.0 |
DBConveyorNode |
Represents DB conveyor node
To create a new instance of this class, use DBNodeManager.createDBConveyorNode(nxopen.Part) Created in NX9.0.0 |
DBFactoryCadGeoNode |
Represents DB import factory cad geo node
To create a new instance of this class, use DBNodeManager.createDBFactoryCadGeoNode(nxopen.Part) Created in NX11.0.0 |
DBFactoryNode |
Represents DB factory node
To create a new instance of this class, use DBNodeManager.createDBFactoryNode(nxopen.Part, nxopen.linedesigner.DBFactoryNode.NodeType) Created in NX9.0.0 |
DBFenceNode |
Represents DB factory node
To create a new instance of this class, use DBNodeManager.createDBFenceNode(nxopen.Part) Created in NX9.0.0 |
DBFloorEquipmentNode |
Represents DB Floor equipment node
To create a new instance of this class, use DBNodeManager.createDBFloorEquipmentNode(nxopen.Part) Created in NX9.0.0 |
DBNode |
Represents DB node
This is an abstract class, and cannot be instantiated. |
DBNodeContainer |
Represents DB node container
To create a new instance of this class, use DBNodeManager.createDBNodeContainer(nxopen.Part) Created in NX9.0.0 |
DBNodeManager |
Represents a manager of line designer db nodes
Use the static method in this class to obtain an instance. |
DBNodeUtils |
Represents a utils of line designer for journaling uinode methods
Use the static method in this class to obtain an instance. |
DBPlatformEquipmentNode |
Represents DB platform equipment node
To create a new instance of this class, use DBNodeManager.createDBPlatformEquipmentNode(nxopen.Part) Created in NX9.0.0 |
DBSmartComplexEquipmentNode |
Represents DB factory node .
|
DBSmartEquipmentNode |
Represents DB factory node .
|
DBStairwayEquipmentNode |
Represents DB stairway equipment node
To create a new instance of this class, use DBNodeManager.createDBStairwayEquipmentNode(nxopen.Part) Created in NX9.0.0 |
DiamondConnectorFeature |
Represents a typed connector feature feature
To create or edit an instance of this class, use TypedConnectorFeatureBuilder Created in NX9.0.0 |
DisconnectConnectionBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createDisconnectConnectionBuilder Created in NX10.0.0 |
ExportPlantToDWG |
Represents the export plant to dwg
To create or edit an instance of this class, use ExportPlantToDWGBuilder Created in NX9.0.0 |
ExportPlantToDWGBuilder |
Represents a
LineDesigner.ExportPlantToDWG builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createExportPlantToDwgBuilder Default values. |
ExportToDWG |
Represents an export to dwg
To create or edit an instance of this class, use ExportToDWGBuilder Created in NX9.0.0 |
ExportToDWGBuilder |
Represents a
LineDesigner.ExportToDWG builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createExportToDwgBuilder Default values. |
FastPlacementUtilityBuilder |
Fast Placement
Established by LineDesigner_LineDesignerManager whenever it is needed. |
FloorEquipmentBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createFloorequipmentBuilder Default values. |
GateFeature |
Represents a gate feature
To create or edit an instance of this class, use GateFeatureBuilder Created in NX9.0.0 |
GateFeatureBuilder |
Represents a
LineDesigner.GateFeature builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createGateFeatureBuilder Default values. |
GlobalSelectionBuilder |
Global Selection
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createGlobalSelectionBuilder Created in NX9.0.0 |
HeadConnectorFeature |
Represents a typed connector feature feature
To create or edit an instance of this class, use TypedConnectorFeatureBuilder Created in NX9.0.0 |
HoleFeature |
Represents a hole feature feature
To create or edit an instance of this class, use HoleFeatureBuilder Created in NX9.0.0 |
HoleFeatureBuilder |
Represents a
LineDesigner.HoleFeature builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createHoleFeatureBuilder Default values. |
ImportFactoryCadGeoBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createImportFactoryCadGeoBuilder Created in NX10.0.0 |
InsertSheet |
Represents an insert sheet
To create or edit an instance of this class, use InsertSheetBuilder Created in NX9.0.0 |
InsertSheetBuilder |
Represents a
LineDesigner.InsertSheet builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createInsertSheetBuilder Default values. |
JigOnPlaneBuilder |
Jig on plane
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createJigOnPlaneBuilder Created in NX9.0.0 |
LineDesignerApplicationBuilder |
Represents a class to create enter and exit the LineDesigner application
.
|
ModelBaseObject |
Represents Model Base Object
This is an abstract class, and cannot be instantiated. |
ModelPlantManager |
Represents a manager of line designer model
Use the static method in this class to obtain an instance. |
ModelPlantRoot |
Represents a manager of line designer plant model
Established by LineDesigner_ModelPlantManager when we enter the application . |
ModelProductionUnit |
Represents Production Unit .
|
ModelResourceInstance |
Represents Resource Instance .
|
PickRectanglePointsBuilder |
Pick Rectangle Points
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createPickRectanglePointsBuilder Created in NX9.0.0 |
PlanViewManager |
Represents a singleton JA for PlanViewManager
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createPlanViewManagerInstance Created in NX9.0.0 |
PlatformEquipmentBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createPlatformEquipmentBuilder Default values. |
ProductionUnitCreatorBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createProductionUnitCreatorBuilder Created in NX10.0.0 |
RailingFeature | |
RailingFeatureBuilder |
Represents a
LineDesigner.RailingFeature Features.FeatureBuilder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createRailingFeatureBuilder Default values. |
RailOpeningFeature |
Represents a rail Opening feature
To create or edit an instance of this class, use RailOpeningFeatureBuilder Created in NX9.0.0 |
RailOpeningFeatureBuilder |
Represents a
LineDesigner.RailOpeningFeature builder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createRailOpeningFeatureBuilder Default values. |
RenameItemRevisionBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createRenameItemRevisionBuilder Created in NX10.0.3 |
ResizeConnectorBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createResizeConnectorBuilder Default values. |
ReuseLibraryDragData |
Represents a manager of line designer plant model
Established by LineDesigner_ReuseLibraryUtilityBuilder whenever it is needed. |
ReuseLibraryUtilityBuilder |
Represents a JA for ReuseLibraryUtility
Established by LineDesigner_LineDesignerManager whenever it is needed. |
SingleElementConveyorBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createSingleElementConveyorBuilder Created in NX9.0.0 |
StairwayEquipmentBuilder |
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createStairwayEquipmentBuilder Default values. |
TailConnectorFeature |
Represents a typed connector feature feature
To create or edit an instance of this class, use TypedConnectorFeatureBuilder Created in NX9.0.0 |
TypedConnectorFeature |
Represents a typed connector feature feature
To create or edit an instance of this class, use TypedConnectorFeatureBuilder Created in NX9.0.0 |
TypedConnectorFeatureBuilder |
Represents a
LineDesigner.TypedConnectorFeature Features.FeatureBuilder
To create a new instance of this class, use nxopen.linedesigner.LineDesignerManager#createTypedConnectorFeatureBuilder Default values. |
UINodeUtils |
Represents a utils of line designer for journaling uinode methods
Use the static method in this class to obtain an instance. |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.