Interface | Description |
---|---|
AssemblyCreationSettingsBuilder | |
AssemblyFromLayout2dBuilder |
Represents a Builder for create assembly from Layout functionality which will create a
new assembly from the selected Layout
To create a new instance of this class, use ComponentCollection.createAssemblyFromLayout2dBuilder() Created in NX10.0.0 |
Component |
Represents the Component object.
|
ComponentCollection |
Represents a collection of
Component s. |
ComponentDefinition |
Represents a component definition.
|
ComponentDefinitionCollection |
Represents a collection of
ComponentDefinition objects. |
ComponentNameBuilder |
This class is used to construct the component name and part file name block, if it is in
manage mode, we also have item number, item revision and item name .
|
ComponentSettingsBlockBuilder |
Represents the Component Settings Button (Layout2d.ComponentSettingsBlockBuilder)
Created in NX10.0.0 |
ComponentSettingsBuilder |
Represents a
ComponentSettingsBuilder
This builder stores the information of the 2D Component settings
Created in NX10.0.0 |
CreateComponentFrom3DBuilder |
Represents a Builder for CreateComponentFrom3DBuilder functionality which will define
To create a new instance of this class, use ComponentCollection.createComponentFrom3dBuilder(nxopen.View) Default values. |
CreateComponentFrom3DSettingsBuilder | |
DefineComponentAnchorPointBuilder |
Represents a Builder for Define Component Anchor Point functionality which will define the anchor
point location of a 2D Component instance
To create a new instance of this class, use ComponentCollection.createDefineComponentAnchorPointBuilder() Created in NX10.0.0 |
DefineComponentBuilder |
Represents a Builder for Define 2D component functionality which will define
a 2D Component and stores its definition in the Reuse Library
To create a new instance of this class, use ComponentCollection.createDefineComponentBuilder(nxopen.layout2d.Component) Default values. |
EditComponentSettingsBuilder |
Represents a
EditComponentSettingsBuilder builder. |
ExportComponentHierarchyBuilder |
Represents a Builder for export component 2D hierarchy
To create a new instance of this class, use ComponentCollection.createExportComponentHierarchyBuilder() Created in NX11.0.0 |
InsertComponentBuilder |
Represents a Builder for Insert Component functionality which will insert a 2D
Component instance in the active sketch
To create a new instance of this class, use ComponentCollection.createInsertComponentBuilder() Created in NX10.0.0 |
LocalDefinitionFolder |
Represents a local definition folder.
|
LocalDefinitionFolderBuilder |
Represents a
LocalDefinitionFolderBuilder . |
LocalDefinitionFolderCollection |
Represents a collection of
LocalDefinitionFolder objects. |
MakeComponentUniqueBuilder |
Represents a Builder for Make 2D Component unique functionality which will create a
new definition of the selected 2D Component instance
To create a new instance of this class, use ComponentCollection.createMakeComponentUniqueBuilder() Default values. |
NewComponentBuilder |
Represents a Builder for New 2D Component functionality which will create an empty 2D Component
instance and stores its definition in the local 2D Component folder
To create a new instance of this class, use ComponentCollection.createNewComponentBuilder() Created in NX10.0.0 |
PublishComponentBuilder |
Represents a Builder for Publish 2D Component functionality which will allow
local definitions to be exported into external storage locations
To create a new instance of this class, use ComponentCollection.createPublishComponentBuilder() Created in NX10.0.0 |
ReparentComponentBuilder |
Represents a Builder for Reparent 2D Component functionality which will reparents
the selected 2D Component contents from another 2D Component definition.
|
ReplaceComponentBuilder |
Represents a Builder for Replace 2D Component functionality which will replaces
the selected 2D Component contents from another 2D Component definition.
|
SelectComponent |
Represents a single object selection.
|
SelectComponentList |
Represents a list of objects on a selection list.
|
SmashComponentBuilder |
Represents a Builder for Smash 2D Component functionality which will break instances
of 2D Components into its constituent pieces, we can have multiple committed objects
To create a new instance of this class, use ComponentCollection.createSmashComponentBuilder() Created in NX10.0.0 |
Class | Description |
---|---|
Component.AnchorPointData |
This class holds the data returned from
Component.getAnchorPoint() |
Component.TransformData |
This class holds the data returned from
Component.getTransform() |
CreateComponentFrom3DBuilder.CreateMethod |
the method to use
|
CreateComponentFrom3DBuilder.ProjectionPlaneData |
This class holds the data returned from
CreateComponentFrom3DBuilder.getProjectionPlane() |
Layout2dComponentMemberType |
Component member type
|
Layout2dDefinitionLocation |
Definition location
|
Layout2dDefinitionStatus |
Definition Status
|
SelectComponent.ValueData |
This class holds the data returned from
SelectComponent.getValue() |
SelectComponent.ValueWithCaeSetObjectInfoData |
This class holds the data returned from
SelectComponent.getValue() |
SelectComponent.ValueWithSnapData |
This class holds the data returned from
SelectComponent.getValue() |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.