public static class PlatformEquipmentBuilder.DeckSupportTypeAPI extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_AUTOMATIC_SUPPORTIN_GRID_PATTERN |
static int |
_CORNERS_SUPPORTS_ONLY |
static int |
_MANUAL_SUPPORTS |
static int |
_NO_SUPPORTS |
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
AUTOMATIC_SUPPORTIN_GRID_PATTERN |
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
CORNERS_SUPPORTS_ONLY |
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
MANUAL_SUPPORTS |
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
NO_SUPPORTS |
Modifier and Type | Method and Description |
---|---|
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PlatformEquipmentBuilder.DeckSupportTypeAPI |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PlatformEquipmentBuilder.DeckSupportTypeAPI[] |
values()
Returns an array that contains the values for this enum.
|
public static final PlatformEquipmentBuilder.DeckSupportTypeAPI NO_SUPPORTS
public static final PlatformEquipmentBuilder.DeckSupportTypeAPI CORNERS_SUPPORTS_ONLY
public static final PlatformEquipmentBuilder.DeckSupportTypeAPI AUTOMATIC_SUPPORTIN_GRID_PATTERN
public static final PlatformEquipmentBuilder.DeckSupportTypeAPI MANUAL_SUPPORTS
public static final int _NO_SUPPORTS
public static final int _CORNERS_SUPPORTS_ONLY
public static final int _AUTOMATIC_SUPPORTIN_GRID_PATTERN
public static final int _MANUAL_SUPPORTS
public static PlatformEquipmentBuilder.DeckSupportTypeAPI valueOf(int value)
public static PlatformEquipmentBuilder.DeckSupportTypeAPI valueOf(String name)
public static PlatformEquipmentBuilder.DeckSupportTypeAPI[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.