Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.annotations |
Provides classes and interfaces relating to Dimensions, Notes, Symbols, PMI, and other Annotations.
|
nxopen.gateway |
Provides classes and interfaces for Gateway.
|
nxopen.layout2d |
Provides classes and interfaces for Layout2D.
|
Class and Description |
---|
BookmarkFile
Represents operations which can be done on bookmark files.
|
CopyCutBuilder
Represents a
CopyCutBuilder
To create a new instance of this class, use ClipboardOperationsManager.createCopyCutBuilder() Created in NX7.5.0 |
GenericFileNewBuilder
Represents a builder class that performs Generic File New operations.
|
ImageCaptureManager
the ImageCaptureManager class
To obtain an instance of this class, refer to BasePart Created in NX7.5.0 |
PasteBuilder
Represents a
PasteBuilder
To create a new instance of this class, use ClipboardOperationsManager.createPasteBuilder() Created in NX7.5.0 |
Class and Description |
---|
BaseExplicitOrderBuilder
This is the
BaseExplicitOrderBuilder for the explicit order This is an abstract class, and cannot be instantiated. |
ImageCaptureBuilder
Represents a
ImageCaptureBuilder builder To create a new instance of this class, use ImageCaptureManager.createImageCaptureBuilder() Default values. |
Class and Description |
---|
CopyCutBuilder.Status
Status of Copy or Cut Operation
|
IGenericFileNewApplicationBuilder
Represents the class Application Builder.
|
ImageCaptureBuilder
Represents a
ImageCaptureBuilder builder To create a new instance of this class, use ImageCaptureManager.createImageCaptureBuilder() Default values. |
ImageCaptureBuilder.CaptureMethodType
the selection method
|
ImageCaptureBuilder.ImageFormat
the image format
|
ImageCaptureBuilder.ImageSize
the image size
|
ImageCaptureBuilder.RegionData
This class holds the data returned from
ImageCaptureBuilder.getRegion() |
Class and Description |
---|
ImageCaptureBuilder
Represents a
ImageCaptureBuilder builder To create a new instance of this class, use ImageCaptureManager.createImageCaptureBuilder() Default values. |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.