Interface | Description |
---|---|
BaseExplicitOrderBuilder |
This is the
BaseExplicitOrderBuilder for the explicit order This is an abstract class, and cannot be instantiated. |
BookmarkFile |
Represents operations which can be done on bookmark files.
|
CopyCutBuilder |
Represents a
CopyCutBuilder
To create a new instance of this class, use ClipboardOperationsManager.createCopyCutBuilder() Created in NX7.5.0 |
GenericFileNewBuilder |
Represents a builder class that performs Generic File New operations.
|
IGenericFileNewApplicationBuilder |
Represents the class Application Builder.
|
ImageCaptureBuilder |
Represents a
ImageCaptureBuilder builder To create a new instance of this class, use ImageCaptureManager.createImageCaptureBuilder() Default values. |
ImageCaptureManager |
the ImageCaptureManager class
To obtain an instance of this class, refer to BasePart Created in NX7.5.0 |
PasteBuilder |
Represents a
PasteBuilder
To create a new instance of this class, use ClipboardOperationsManager.createPasteBuilder() Created in NX7.5.0 |
Class | Description |
---|---|
CopyCutBuilder.Status |
Status of Copy or Cut Operation
|
ImageCaptureBuilder.CaptureMethodType |
the selection method
|
ImageCaptureBuilder.ImageFormat |
the image format
|
ImageCaptureBuilder.ImageSize |
the image size
|
ImageCaptureBuilder.RegionData |
This class holds the data returned from
ImageCaptureBuilder.getRegion() |
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.