public static class EmbossLimit.EndcapSourceOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_FACE
Indicates the geometries are selected surfaces not on the target.
|
static int |
_PLANE
Indicates the geometry is datum plane.
|
static int |
_SECTION
Indicates the geometry is the sketch plane on which the section resides.
|
static int |
_TARGET
Indicates the geometries are some of the faces on the Target Body.
|
static EmbossLimit.EndcapSourceOption |
FACE
Indicates the geometries are selected surfaces not on the target.
|
static EmbossLimit.EndcapSourceOption |
PLANE
Indicates the geometry is datum plane.
|
static EmbossLimit.EndcapSourceOption |
SECTION
Indicates the geometry is the sketch plane on which the section resides.
|
static EmbossLimit.EndcapSourceOption |
TARGET
Indicates the geometries are some of the faces on the Target Body.
|
Modifier and Type | Method and Description |
---|---|
static EmbossLimit.EndcapSourceOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossLimit.EndcapSourceOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossLimit.EndcapSourceOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final EmbossLimit.EndcapSourceOption TARGET
public static final EmbossLimit.EndcapSourceOption PLANE
public static final EmbossLimit.EndcapSourceOption SECTION
public static final EmbossLimit.EndcapSourceOption FACE
public static final int _TARGET
public static final int _PLANE
public static final int _SECTION
public static final int _FACE
public static EmbossLimit.EndcapSourceOption valueOf(int value)
public static EmbossLimit.EndcapSourceOption valueOf(String name)
public static EmbossLimit.EndcapSourceOption[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.