public static class EmbossLimit.EndcapMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
Indicates End-Cap geometry is formulated by the selected geometry without displacement.
|
static int |
_OFFSET_APPROXIMATION
Indicates End-Cap geometry is formulated as an approximate offset of the selected End-Cap geometry
|
static int |
_OFFSET_EXACT
Indicates End-Cap geometry is formulated as an exact offset of the selected End-Cap geometry.
|
static int |
_TRANSLATION
Indicates End-Cap geometry is a translation along a user controlled vector.
|
static EmbossLimit.EndcapMethod |
NONE
Indicates End-Cap geometry is formulated by the selected geometry without displacement.
|
static EmbossLimit.EndcapMethod |
OFFSET_APPROXIMATION
Indicates End-Cap geometry is formulated as an approximate offset of the selected End-Cap geometry
|
static EmbossLimit.EndcapMethod |
OFFSET_EXACT
Indicates End-Cap geometry is formulated as an exact offset of the selected End-Cap geometry.
|
static EmbossLimit.EndcapMethod |
TRANSLATION
Indicates End-Cap geometry is a translation along a user controlled vector.
|
Modifier and Type | Method and Description |
---|---|
static EmbossLimit.EndcapMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EmbossLimit.EndcapMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EmbossLimit.EndcapMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final EmbossLimit.EndcapMethod TRANSLATION
public static final EmbossLimit.EndcapMethod OFFSET_EXACT
public static final EmbossLimit.EndcapMethod OFFSET_APPROXIMATION
public static final EmbossLimit.EndcapMethod NONE
public static final int _TRANSLATION
public static final int _OFFSET_EXACT
public static final int _OFFSET_APPROXIMATION
public static final int _NONE
public static EmbossLimit.EndcapMethod valueOf(int value)
public static EmbossLimit.EndcapMethod valueOf(String name)
public static EmbossLimit.EndcapMethod[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.