public interface PostGraphAlongPathBuilder extends PostGraphBuilder
PostGraphAlongPathBuilder
Property | Value |
---|---|
QueryCurveUsageOptions.CurveUsage | UseVertices |
QueryCurveUsageOptions.DistanceTolerance | 0 |
QueryCurveUsageOptions.ResultantCurveLocator | UseAsIs |
QueryCurveUsageOptions.ResultantLocationTolerance | 0 |
Modifier and Type | Interface and Description |
---|---|
static class |
PostGraphAlongPathBuilder.CoordinateSysAxis
options for defining the specific coordinate system axis to be used
|
static class |
PostGraphAlongPathBuilder.CsysType
csys types
|
static class |
PostGraphAlongPathBuilder.Xaxis
select option to define the path as x axis
|
PostGraphBuilder.DataErrorHandling, PostGraphBuilder.EdgeIntegralOption, PostGraphBuilder.EntityType, PostGraphBuilder.EvalutionErrors, PostGraphBuilder.FaceIntegralOption, PostGraphBuilder.GeometryValue, PostGraphBuilder.IncompatibleResult, PostGraphBuilder.NodalCombination
Modifier and Type | Method and Description |
---|---|
PostGraphAlongPathBuilder.CoordinateSysAxis |
csysAxis()
Returns the option to define the coordinate system axis to be used when x axis defined by
PostGraphAlongPathBuilder.Xaxis.COORDINATE_VALUE_OF_COORDINATE_SYSTEM_AXIS
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") Created in NX9.0.0 |
boolean |
defineByPathOption()
Returns a value indicating whether the x axis is define by a path ID.
|
boolean |
includeItersectionsOption()
Returns the value indicating whether to include intersections points while defining the x axis along the path
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
int |
pathId()
Returns the path id to define the x axis with path
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
QueryCurveUsageOptions |
queryCurveUsageOptions()
Returns the query curve usage options
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setCsys(Matrix3x3 csys)
Set csys for extracting data for x axis
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setCsysAxis(PostGraphAlongPathBuilder.CoordinateSysAxis axis)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setCsysType(PostGraphAlongPathBuilder.CsysType csystype)
Sets csys type for extracting abscissa
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setDefineByPathOption(boolean defineByPath)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setIncludeItersectionsOption(boolean includeItersections)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setOrigin(Point3d origin)
Set vector origin for extracting data for x axis
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setPathId(int pathId)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setVector(Point3d unitvector)
Set vector for extracting data for x axis
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
setXaxisOption(PostGraphAlongPathBuilder.Xaxis xaxis)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
PostGraphAlongPathBuilder.Xaxis |
xaxisOption()
Returns the option for defining the x axis of the graph.
|
complexGraphTypes, createFieldOption, edgeIntegralOptionValue, evalutionErrorsOption, faceIntegralOptionValue, geometryCombinationValue, getFieldTable, graphTitle, incompatibleResultOption, nodalCombinationValue, noDataOption, saveAfuOption, selectedEntityType, setComplexGraphTypes, setCreateFieldOption, setEdgeIntegralOptionValue, setEntityIds, setEntityObjects, setEvalutionErrorsOption, setFaceIntegralOptionValue, setFreePoints, setGeometryCombinationValue, setGraphTitle, setIncompatibleResultOption, setNodalCombinationValue, setNoDataOption, setSaveAfuOption, setSelectedEntityType, setUserData, userData
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
PostGraphAlongPathBuilder.Xaxis xaxisOption() throws NXException, RemoteException
PostGraphAlongPathBuilder.Xaxis.COORDINATE_VALUE_OF_COORDINATE_SYSTEM_AXIS
is set use
setCsys(nxopen.Matrix3x3)
, setCsysType(nxopen.cae.PostGraphAlongPathBuilder.CsysType)
needs to be used to specify csys and csys type and use csysAxis()
and setCsysAxis(nxopen.cae.PostGraphAlongPathBuilder.CoordinateSysAxis)
If the option PostGraphAlongPathBuilder.Xaxis.LENGTH_ALONG_DIRECTION
is set use
setOrigin(nxopen.Point3d)
, setVector(nxopen.Point3d)
need to be used to specify vector along which length of the path points will be calculated
NXException
RemoteException
void setXaxisOption(PostGraphAlongPathBuilder.Xaxis xaxis) throws NXException, RemoteException
xaxis
- NXException
RemoteException
PostGraphAlongPathBuilder.CoordinateSysAxis csysAxis() throws NXException, RemoteException
PostGraphAlongPathBuilder.Xaxis.COORDINATE_VALUE_OF_COORDINATE_SYSTEM_AXIS
NXException
RemoteException
void setCsysAxis(PostGraphAlongPathBuilder.CoordinateSysAxis axis) throws NXException, RemoteException
axis
- NXException
RemoteException
boolean defineByPathOption() throws NXException, RemoteException
pathId()
and setPathId(int)
NXException
RemoteException
void setDefineByPathOption(boolean defineByPath) throws NXException, RemoteException
defineByPath
- NXException
RemoteException
int pathId() throws NXException, RemoteException
NXException
RemoteException
void setPathId(int pathId) throws NXException, RemoteException
pathId
- NXException
RemoteException
boolean includeItersectionsOption() throws NXException, RemoteException
NXException
RemoteException
void setIncludeItersectionsOption(boolean includeItersections) throws NXException, RemoteException
includeItersections
- NXException
RemoteException
void setVector(Point3d unitvector) throws NXException, RemoteException
unitvector
- NXException
RemoteException
void setCsys(Matrix3x3 csys) throws NXException, RemoteException
csys
- NXException
RemoteException
void setOrigin(Point3d origin) throws NXException, RemoteException
origin
- NXException
RemoteException
void setCsysType(PostGraphAlongPathBuilder.CsysType csystype) throws NXException, RemoteException
csystype
- set csys typeNXException
RemoteException
QueryCurveUsageOptions queryCurveUsageOptions() throws NXException, RemoteException
NXException
RemoteException
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.