public static class PostGraphBuilder.DataErrorHandling extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_SKIP |
static int |
_USER_VALUE
User given value will used for those entities which do not have result value associated with them
|
static PostGraphBuilder.DataErrorHandling |
SKIP |
static PostGraphBuilder.DataErrorHandling |
USER_VALUE
User given value will used for those entities which do not have result value associated with them
|
Modifier and Type | Method and Description |
---|---|
static PostGraphBuilder.DataErrorHandling |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PostGraphBuilder.DataErrorHandling |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PostGraphBuilder.DataErrorHandling[] |
values()
Returns an array that contains the values for this enum.
|
public static final PostGraphBuilder.DataErrorHandling SKIP
public static final PostGraphBuilder.DataErrorHandling USER_VALUE
public static final int _SKIP
public static final int _USER_VALUE
public static PostGraphBuilder.DataErrorHandling valueOf(int value)
public static PostGraphBuilder.DataErrorHandling valueOf(String name)
public static PostGraphBuilder.DataErrorHandling[] values()
Copyright 2016 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.